AM62x MCU+ SDK  12.00.00
Software Diagnostics Library (SDL)

Introduction

The AM62X family of SoCs provides various safety mechanisms and features, as well as recommendations for usage of these safety mechanisms and features. The Software Diagnostic Library (SDL) provides interfaces to these safety mechanisms and features. SDL provides these interfaces to assist in the development of software applications involving Functional Safety.

In an application involving functional safety, the detection of random hardware faults and ability to take the appropriate response to get the system to a safe state is of utmost importance. Methods to detect and respond to faults in a system are called functional safety mechanisms or safety functions. Examples of safety mechanisms available on an SoC include error correction/detection (ECC) on memory regions, Error Signaling Module (ESM) to monitor error events, etc.

The safety-critical processor product family provides various hardware functional safety mechanisms. For example, this software release provides an API to configure ECC and a reference example to set up interrupts to check on ECC error events detected by hardware. Overall, the system integrator can use this API and implement software diagnostics to meet the safety system goals.

The user of this document should have a general familiarity with the safety-critical processor family.

The Software Diagnostics Library consists of different blocks for Error Capture and Safety Mechanisms. Error response is managed by the Application based on the device Safety Manual requirements. The interface for the Application is in the form of software APIs. The following diagram shows the high-level blocks of the SDL as well as the overall system. The application may use either no OS or an OS. In the diagram an OS is shown as an example only. This is an overview and does not list all the IPs supported as part of the SDL.

In the following diagram, the green blocks represent the scope of the SDL. The dark blue is the application, and the light blue represents external modules used by the application along with SDL.

SDL Architecture

The Software Diagnostics Library provides the functionality for implementing hardware safety mechanisms that can be run during the various operation modes of the device. The functions of the SDL which are used by the application during the various modes are as follows:

  • Startup of device
    • Self-test diagnostics to verify correct operation of the device
    • SDL APIs to initialize continuous diagnostics
  • Runtime
    • Notification of errors detected by the continuous diagnostics through the ESM handler
    • SDL APIs to execute periodic diagnostics

SDL consists of below sub-modules

Compliance Support package (CSP)

The SDL Compliance Support Package (CSP) was developed to provide the necessary documentation and reports to assist customers using SDL to comply with functional safety standards. The CSP provides software architecture and design documents for the SDL along with software quality reports like detailed static and dynamic analysis reports. It also provides traceability report and test reports that correlate the requirements and results from formal tests used to test the safety feature. The CSP can be requested through MySecureSW from the below link:

Request CSP

The full list of collateral included in CSP packages is provided below:

Requirements and Design

  • Software Product Specification: This document details the software product specification of SDL.
  • Architecture Document: This document describes the software architecture of SDL.
  • AM62X Detailed Design Document: This document describes the software design of SDL in AM62X.
  • Functional Safety Impact Analysis Document: This document identifies the amount of reuse from previous certified Sitara MPU SDL version, detailing all the requirements that are reused, deleted and added for all SoCs.

Test Reports and Result

  • Static Analysis Report: This report provides summary of the Software quality metrics and the MISRA-C 2004 violations.
  • Dynamic Analysis Report: This report provides summary of the Structural Coverage metrics (Statement, Branch Coverage metrics).
  • Test Report: This report provides detailed information about the results of the formal testing.
  • Traceability Report: This report provides the traceability matrix between different phases of software development.
  • Datasheet: This document provides profiling data (timing) of various APIs used in SDL and the memory footprints of SDL source files

Safety Documentation and Process Compliance

  • Software Safety Manual: This document is a functional safety manual for SDL.
  • Software FMEA: This document is the FMEA document for SDL.
  • Evidence of Process Compliance: This includes Phase End Audits for all the 4 phases of SDL's development, acting as proof that all necessary safety compliant processes were followed during the development
  • Others: Other documents such as the MCU-PLUS-SDK Manifest and the list of checksums of SDL Source files are also included

Documentation on TI.com

Other official documentation for your device, such as User Guide, Errata, TÜV SÜD SDL certification (for applicable devices) etc. may be found at https://www.ti.com/product/$DEVICE_NAME.

For example, AM62A7 SDL TUV certificate can be found at https://www.ti.com/product/AM62A7 and then searching for "TUV SUD" in the Technical documentation section.