AM62x MCU+ SDK  12.00.00
Release Notes 10.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62x M4F, R5F, A53 SK-AM62 (referred as am62x-sk in code), SK-AM62-LP (referred as am62x-sk-lp in code), SK-AM62-SIP (referred as am62x-sip-sk in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Attention
DeepSleep low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. This is because when the SoC goes to any LPM, the context of peripherals used by DM R5 will be lost. To use DM R5 for a general purpose application, disable LPM support. Refer Disabling Low Power Mode to know how to disable LPM.
Feature Module
Bad block management support for OSPI NAND OSPI
A53 Drivers: ECAP, EPWM, EQEP, GPMC, Spinlock Drivers
GPIO default value can be configured in sysconfig GPIO
GPIO direction is set part of sysconfig generated code GPIO
FreeRTOS FAT is now supported with FreeRTOS File System
QoS support QoS
Early PLL driver in TIFS init updated to follow recommended sequence to avoid PLL instability TIFS
PM PLL and HSDIV programing in PLL init updated to remove steps violating the recommendation DM

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
A53 FreeRTOS support and A53 FreeRTOS examples DPL, FreeRTOS

Other Updates on This Release

Update Module
ATF Load Address is updated to 0X80000000 from 0x9e780000 LinuxAppImageGen, QnxAppImagegen
Linux FDT is added in qnx app image and loaded at DDR 0x88000000 QnxAppImagegen
make commands are added in boardcfg makefile to open k3-resource-part tool BoardCfg
OSPI tuning optimizations to redue tuning time OSPI
I2C driver updated for inclusinve API names I2C
Bootloader powers off cores if image not present SBL
FreeRTOS FAT will now work with FreeRTOS application as well FAT FS

FreeRTOS Support on A53

Is Is Not
FreeRTOS single core support on A53 GPU Support
Drivers listed for A53 in "SOC Device Drivers" section Low power mode support
- CSI RX Driver
- WiFi, USB, BLE Drivers
- Safety on A53

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.
Tools/Components Supported CPUs Version
Code Composer Studio M4F, R5F, A53 12.7.0
SysConfig M4F, R5F, A53 1.20.0, build 3587
TI ARM CLANG M4F, R5F 3.2.2.LTS
GCC AARCH64 A53 9.2-2019.12
FreeRTOS Kernel M4F, R5F, A53 10.6.1
TIFS NA 10.00.08

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel M4F, R5F, A53 NA
FreeRTOS POSIX M4F, A53 NA
No RTOS M4F, R5F, A53 NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate M4F, R5F Yes FreeRTOS, NORTOS
Cache R5F, A53 Yes FreeRTOS, NORTOS
Clock M4F, R5F, A53 Yes FreeRTOS, NORTOS
CycleCounter M4F, R5F, A53 NA FreeRTOS, NORTOS
Debug M4F, R5F, A53 Yes FreeRTOS, NORTOS
Heap M4F, R5F, A53 NA FreeRTOS, NORTOS
Hwi M4F, R5F, A53 Yes FreeRTOS, NORTOS
MPU M4F, R5F, A53 Yes FreeRTOS, NORTOS
Semaphore M4F, R5F, A53 NA FreeRTOS, NORTOS
Task M4F, R5F, A53 NA FreeRTOS
Timer M4F, R5F, A53 Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NOR R5F Yes Yes Yes NORTOS
OSPI NAND R5F Yes Yes Yes NORTOS
EMMC R5F Yes NA NA NORTOS
UART R5F Yes NA No NORTOS

SOC Device Drivers

Peripheral Domain Supported CPUs SysConfig Support
DDR Main R5F Yes
ECAP Main A53 Yes
EPWM Main M4F, A53 Yes
EQEP Main A53 Yes
GPIO MCU M4F, R5F Yes
Main M4F, R5F, A53 Yes
GPMC Main R5F, A53 Yes
I2C Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
IPC Main M4F, R5F, A53 Yes
MCAN Main R5F, A53 Yes
MCU M4F Yes
MCSPI Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
MMCSD Main R5F, A53 Yes
OSPI Main R5F, A53 Yes
Pinmux Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
SOC NA M4F, R5F, A53 Yes
SCIClient NA M4F, R5F, A53 Yes
UART Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup R5F Yes
UDMA Main R5F, A53 Yes
WDT Main A53 Yes
Note
Refer Accessing main and wakeup domain peripherals from MCU domain for accessing main/wakeup peripherals from MCU Domain.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
Flash R5F Yes

Software Diagnostic Library (SDL)

SDL Module Supported CPUs SysConfig Support
ESM M4F, R5F No
MCRC M4F, R5F No
RTI M4F, R5F No
DCC M4F, R5F No
VTM M4F, R5F No
STOG M4F, R5F No
PBIST M4F, R5F No
MTOG M4F No
POK M4F, R5F No
ECC M4F, R5F No
LBIST M4F No
ROM Checksum R5F No

Fixed Issues

ID Head Line Module Applicable Releases
SITSW-3920 DDR Inline ECC example does not work in debug mode on AM62x DDR 09.01.00 onwards
SITSW-3945 Issues with the OSPI NAND PHY tuning OSPI 09.00.00 onwards
SITSW-4229 OSPI NAND performance reduction when phy tuning is skipped OSPI 09.02.00 onwards
SITSW-4271 Update the FSS_CTRL register to support 128MB flash size by default. OSPI 09.01.00 onwards
SITSW-4282 Skip tuning is not happenning for sbl stage2 as stage1 closes the drivers. OSPI 09.01.00 onwards
SITSW-4337 Bootloader_socInitR5FAtcmBtcm function uses global ATCM address resulting in CBASS error SBL 08.06.00 onwards
SITSW-4345 A53 core freq is limited to 1250MHz in bootloader SBL 08.06.00 onwards
SITSW-4417 No checks on number blocks in a single MMCSD R/W transaction MMCSD 09.02.00 onwards
SITSW-4549 OSPI Read delay using an older value OSPI 09.02.00 onwards
SITSW-4599 SysConfig Updates to UART Clock Frequency fails to reflect in ti_drivers_config.c UART 08.04.00 onwards
SITSW-4611 Generated tiboot3.bin in SBL examples are copy of GP images instead of HSFS SBL 08.06.00 onwards
SITSW-4612 UART driver is initialized late in the sysconfig generated code UART 08.06.00 onwards
SITSW-4613 Generation of Board Configuration Binary fails for HS-SE device type SBL 08.06.00 onwards
SITSW-4630 Hwip_disable API not working properly on M4F DPL 08.06.00 onwards
SITSW-4647 AM62X : PADCFG offset value is missing for B16 pin Pinmux 08.06.00 onwards
PROC_SDL-7823 Setting trim value for non-Ping pong mode POKs accesses invalid offset SDL 09.02.00 onwards
SYSFW-7536 Sending JTAG unlock certificate to TIFS using T32 JTAG fails TIFS 09.02.01 onwards
SYSFW-7474 Write access from DMA initiators to RA GCFG region results in firewall exception TIFS 08.06.00 onwards
SYSFW-7485 Update the PLL driver in TIFS boot flow to follow correct sequence TIFS 08.06.00 onwards
SYSFW-7463 TISCI_MSG_GET_CLOCK always return Enabled for input clock DM 08.06.00 onwards
SYSFW-7486 PM: Cleanup additional steps in pll init startup routine DM 08.06.00 onwards

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 07.03.00 Use bash for windows as part of git for windows or don't use -j option
SITSW-2269 DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. DM 08.06.00 None.
SITSW-4001 On SK-AM62-SIP, SBL with ECC enabled does not boot linux, when the SDRAM index is set to 13 DDR 09.01.00 None.
SYSFW-5992 Unable to set exact pixel clock for OLDI LCD display / HDMI Pixel clock DM 08.05.00 Avoid gving range for SET_CLOCK, use exact values for min, max and target
SYSFW-6369 DM unable to enter deep sleep mode when booting in SBL flow DM 08.03.00 None.
SYSFW-6432 Set device API doesn't return Error when PD is in transition state DM 08.03.00 None.
SYSFW-6426 Ownership of a firewall region can be transferred to an invalid host TIFS 08.03.00 None.
SYSFW-7559 LPM: In MCU Only mode resume path the MCU_M4 LPSC is ON DM 10.00.00 None.
SYSFW-7571 LPM: Device IDs higher than 255 will not work with set device constraint DM 10.00.00 None.
PROC_SDL-8404 ECC is not supported for some instances. These are SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR SDL 10.00.00 None. Support will be added in future release.
PROC_SDL-8139 SDL ECC example application exits with failure on UC-2 SDL 10.00.00 Update the MPU config for the example to make the register region as Strongly Ordered. The Example app will be fixed in future release.
PROC_SDL-8138 VTM example app fails when built for freertos SDL 10.00.00 Use the nortos example. Example will be fixed in future release.
PROC_SDL-8137 PBIST example app fails when built for freertos SDL 10.00.00 Use the nortos example. Freertos example will be fixed in future release.
PROC_SDL-8134 POK example app fails when built for freertos SDL 10.00.00 Use the nortos example. Freertos example will be fixed in future release.

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 PHY mode not supported for OSPI NAND SBL on DDR mode. It is supported for SDR mode only Bootloader
3 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Compiler Options

Module Affected API Change Additional Remarks

Examples

Module Affected API Change Additional Remarks

OS Kernel

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks
Bootloader Bootloader_parseAndLoadLinuxAppImage Bootloader_parseAndLoadLinuxAppImage is removed, Bootloader_parseMultiCoreAppImage is updated to parse and load Linux AppImage NA

Networking

Module Affected API Change Additional Remarks