AM62x MCU+ SDK  12.00.00
SDL ECC SEC

Introduction

This example takes an aggregator index as input from the user and performs single bit error test for the corresponding aggregator. It involves the following steps:

  • Setup of an ESM application callback to receive Single Error Correction (SEC) and setup of ECC Aggregators in general
  • Triggering of ECC events for all the RAM IDs, including Interconnect type and Wrapper type
  • Printing out error information within the ECC callback upon reception of ECC events

Aggregators Supported

The following aggregators can be tested using this example.

Aggregator Index ECC Aggregator
0 SDL_COMPUTE_CLUSTER0_SAM62_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE0
1 SDL_COMPUTE_CLUSTER0_SAM62_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE1
2 SDL_COMPUTE_CLUSTER0_SAM62_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE2
3 SDL_COMPUTE_CLUSTER0_SAM62_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE3
4 SDL_COMPUTE_CLUSTER0_SAM62_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_COREPAC
5 SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR
6 SDL_DMASS0_DMSS_AM62_ECCAGGR
7 SDL_ECC_AGGR0_SAM62_SEC_ECC_AGGR
8 SDL_FSS0_FSS_UL_OSPI0_OSPI_WRAP_ECC_AGGR
9 SDL_GICSS0_GIC500SS_1_4_ECC_AGGR
10 SDL_ICSSM0_ICSS_M_CORE_BORG_ECC_AGGR
11 SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR
12 SDL_MCU_ECC_AGGR0_SAM62_MCU_ECC_AGGR
13 SDL_MCU_M4FSS0_BLAZAR_ECC
14 SDL_MCU_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR
15 SDL_MCU_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR
16 SDL_MMCSD0_EMMCSD8SS_ECC_AGGR_RXMEM
17 SDL_MMCSD0_EMMCSD8SS_ECC_AGGR_TXMEM
18 SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_RXMEM
19 SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_TXMEM
20 SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_RXMEM
21 SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_TXMEM
22 SDL_PDMA0_SAM62_PDMA_SPI_ECCAGGR
23 SDL_PDMA1_SAM62_PDMA_UART_ECCAGGR
24 SDL_PSRAMECC_16K0_PSRAM16KX32E_ECC_AGGR
25 SDL_PSRAMECC0_PSRAM256X32E_ECC_AGGR
26 SDL_SA3_SS0_SA3SS_AM62_DMSS_ECCAGGR
27 SDL_SA3_SS0_SA3SS_AM62_SA_UL_ECC_AGGR
28 SDL_SMS0_SMS_HSM_ECC
29 SDL_SMS0_SMS_TIFS_ECC
30 SDL_USB0_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR
31 SDL_USB1_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR
32 SDL_WKUP_ECC_AGGR0_SAM62_DM_ECC_AGGR
33 SDL_WKUP_R5FSS0_PULSAR_UL_CPU0_ECC_AGGR
34 SDL_WKUP_SAFE_ECC_AGGR0_SAM62_WKUP_SAFE_ECC_AGGR
35 SDL_WKUP_VTM0_K3VTM_N16FFC_ECCAGGR
36 SDL_CPSW0_CPSW_3GUSS_CORE_ECC_CPSW_ECC_AGGR

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
m4fss0-0 nortos
Toolchain ti-arm-clang
Board am62x-sk
Example folder examples/sdl/ecc_sec/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run for a couple of aggregators,

[MAIN_Cortex_R5_0_0] Sciclient direct init..... SUCCESS
ECC Example Application
ECC_Test_init: Init MCU ESM complete
ECC_Test_init: Init MAIN ESM complete
ECC_Test_init: ECC Callback Init complete for MCU ESM
ECC_Test_init: ECC Callback Init complete for Main ESM
ECC SDL API tests: starting
Refer the User Guide for the aggregator information
Select the memory to test...
14
...selected 14
ecc_aggrtest: [14] single bit error self test: SDL_MCU_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR starting
ECC_Memory_init: [14] SDL_MCU_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR ECC Init complete
Self test started accessable RamId 0 starting
Self Test completed for accessable RamId 0
Self test started RamId 1 starting
Self test started RamId 1 completed
Select the memory to test...
20
...selected 20
ecc_aggrtest: [20] single bit error self test: SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_RXMEM starting
ECC_Memory_init: [20] SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_RXMEM ECC Init complete
Inject test started not accessable RamId 0 starting
Injected ECC error and got ESM Interrupt
Select the memory to test...