AM62x MCU+ SDK  12.00.00
Coremark-Pro Benchmark

CoreMark®-PRO is a comprehensive, advanced processor benchmark that works with and enhances the market-proven industry-standard EEMBC CoreMark® benchmark. While CoreMark stresses the CPU pipeline, CoreMark-Pro tests the entire processor, adding comprehensive support for multicore technology, a combination of integer and floating-point workloads, and data sets for utilizing larger memory subsystems. The CoreMark-PRO benchmark contains five prevalent integer workloads and four popular floating-point workloads.

The integer workloads include:

  • JPEG compression
  • ZIP compression
  • XML parsing
  • SHA-256 Secure Hash Algorithm
  • A more memory-intensive version of the original CoreMark (CORE)

The floating-point workloads include:

  • Radix-2 Fast Fourier Transform (FFT)
  • Gaussian elimination with partial pivoting derived from LINPACK
  • A simple neural-net
  • A greatly improved version of the Livermore loops benchmark using the following 24 FORTRAN kernels converted to C

Each workload must be compiled individual(as each workload uses different dataset), flashed to the device, verified, and then the score computed manually The CoreMark-PRO score is a weighted geometric mean of each workload

All the workload applications are present in examples/benchmarks/coremark_pro_benchmark folder.

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 freertos
Toolchain arm.gnu.aarch64-none
Boards am62x-sk, am62x-sip-sk, am62x-sk-lp
Example folder examples/benchmarks/coremark_pro_benchmark

Steps to Run the Example

Compute The Overall Score

The score for CoreMark-PRO is a scaled geometric mean of scaled workload scores. Each workload is normalized to a reference value.

The overall score can be computed with the following steps:

  • Change the working directory to {SDK_PATH}/tools/coremarkPro_bechmark.
  • Run the following command with the score obtained from each workload to compute overall benchmark score

    Note
    Change the score according to the workload and use corresponding argument.(–args score)
    python3 coremarkPro.py --core .28 --cjpeg 40.40 --lin 16.30 --loops .71 --parser 5.75 --radix 77.54 --sha 81.72 --zip 27.13 --nnet 1.87

Sample output for Coremark pro benchmark example

- Info: Starting Run...
-- Workload:linear_alg-mid-100x100-sp=1046644201
-- linear_alg-mid-100x100-sp:time(ns)=6134575
-- linear_alg-mid-100x100-sp:contexts=1
-- linear_alg-mid-100x100-sp:iterations=100
-- linear_alg-mid-100x100-sp:time(secs)= 6.13457
-- linear_alg-mid-100x100-sp:secs/workload=0.0613458
-- linear_alg-mid-100x100-sp:workloads/sec= 16.301
-- Done:linear_alg-mid-100x100-sp=1046644201