AM62x MCU+ SDK  11.00.00
Release Notes 11.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62x M4F, R5F, A53 SK-AM62 (referred as am62x-sk in code), SK-AM62-LP (referred as am62x-sk-lp in code), SK-AM62-SIP (referred as am62x-sip-sk in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Attention
DeepSleep low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. This is because when the SoC goes to any LPM, the context of peripherals used by DM R5 will be lost. To use DM R5 for a general purpose application, disable LPM support. Refer Disabling Low Power Mode to know how to disable LPM.
Feature Module
ECC example for R5F cache SDL
IPC between A53 cores IPC
Example for Key Revision update OTP
LPM example for MCU only with Timer and MCAN as wakeup sources LPM
Coremark-pro, Dhrystone, interrupt latency benchmarks for A53 Benchmark
Optimized boottime for eMMC, SD boot by enabling DMA for DDR to DDR copy Bootloader

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
FreeRTOS AMP support on A53. DPL, FreeRTOS
A53 FreeRTOS AMP examples demonstrating usage of ethernet Networking

FreeRTOS Support on A53

Is Is Not
FreeRTOS AMP support on A53 GPU Support
Drivers listed for A53 in "SOC Device Drivers" section Low power mode support
Ethernet Networking CSI RX Driver
- WiFi, USB, BLE Drivers
- Safety on A53

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.
Tools/Components Supported CPUs Version
Code Composer Studio M4F, R5F, A53 20.1.0
SysConfig M4F, R5F, A53 1.23.0, build 4000
TI ARM CLANG M4F, R5F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
FreeRTOS Kernel M4F, R5F, A53 11.1.0

SDK Components

SYSFW / TIFS

Version 11.00.07
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel M4F, R5F, A53 NA
FreeRTOS POSIX M4F, A53 NA
No RTOS M4F, R5F, A53 NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate M4F, R5F Yes FreeRTOS, NORTOS
Cache R5F, A53 Yes FreeRTOS, NORTOS
Clock M4F, R5F, A53 Yes FreeRTOS, NORTOS
CycleCounter M4F, R5F, A53 NA FreeRTOS, NORTOS
Debug M4F, R5F, A53 Yes FreeRTOS, NORTOS
Heap M4F, R5F, A53 NA FreeRTOS, NORTOS
Hwi M4F, R5F, A53 Yes FreeRTOS, NORTOS
MPU M4F, R5F, A53 Yes FreeRTOS, NORTOS
Semaphore M4F, R5F, A53 NA FreeRTOS, NORTOS
Task M4F, R5F, A53 NA FreeRTOS
Timer M4F, R5F, A53 Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NOR R5F Yes Yes Yes NORTOS
OSPI NAND R5F Yes Yes Yes NORTOS
EMMC R5F Yes NA NA NORTOS
UART R5F Yes NA No NORTOS

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN A53 NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP A53 YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver Other LwIP features
Ethernet driver (ENET) A53 YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW RMII mode

SOC Device Drivers

Note
See the updated MCASP usage guidelines in MCASP for changes in MCASP driver
Peripheral Domain Supported CPUs SysConfig Support
DDR Main R5F Yes
DSS Main A53 Yes
ECAP Main A53 Yes
EPWM Main M4F, A53 Yes
EQEP Main A53 Yes
GPIO MCU M4F, R5F Yes
Main M4F, R5F, A53 Yes
GPMC Main R5F, A53 Yes
I2C Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
IPC Main M4F, R5F, A53 Yes
MCAN Main R5F, A53 Yes
MCU M4F Yes
MCSPI Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
MMCSD Main R5F, A53 Yes
OSPI Main R5F, A53 Yes
Pinmux Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup M4F, R5F Yes
RTC Main R5F, A53 Yes
SOC NA M4F, R5F, A53 Yes
SCIClient NA M4F, R5F, A53 Yes
UART Main M4F, R5F, A53 Yes
MCU M4F, R5F Yes
Wakeup R5F Yes
UDMA Main R5F, A53 Yes
WDT Main A53 Yes
Note
Refer Accessing main and wakeup domain peripherals from MCU domain for accessing main/wakeup peripherals from MCU Domain.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
Flash R5F Yes

Software Diagnostic Library (SDL)

SDL Module Supported CPUs SysConfig Support
ESM M4F, R5F No
MCRC M4F, R5F No
RTI M4F, R5F No
DCC M4F, R5F No
VTM M4F, R5F No
STOG M4F, R5F No
PBIST M4F, R5F No
MTOG M4F No
POK M4F, R5F No
ECC M4F, R5F No
LBIST M4F No
ROM Checksum R5F No

Fixed Issues

ID Head Line Module Applicable Releases
EXT_SITMPUSW-52 UART baud rate and operational mode condition misalignment UART 08.03.00
EXT_SITMPUSW-57 Data Abort at MCSPI_udmaIsrTx when using MCSPI DMA MCSPI 08.03.00
EXT_SITMPUSW-58 MCU PLUS SDK: ipc_rpmsg_echo [DM Firmware] Timeout not working as expected, crashes FW DM, IPC 08.03.00
EXT_SITMPUSW-59 VTM giving same value for every call VTM 10.01.00
EXT_SITMPUSW-89 I2C Error Handler transition from status to i2cTransaction.status I2C 08.03.00
EXT_SITMPUSW-90 MMCSD_write & MMCSD_read function fails for the numBlocks greater than 0xFFFF MCSPI 08.04.00
EXT_EP-12318 SDL_ECC_aggrTransBaseAddressTable declared without extern keyword SDL 11.00.00
EXT_EP-12320 AM62x: VTM: vtm_example is failing on R5F core SDL 11.00.00
EXT_EP-12324 gSDL_pvt_poly_golden has to be used in SDL_vtmPrepLookupTable API instead of gSDL_pvt_poly SDL 11.00.00
PROC_SDL-8865 AM62x: ECC: SDL_ICSSM0_ICSS_M_CORE_BORG_ECC_AGGR aggregator is failing SDL 11.00.00
EXT_SITMPUSW-55 AM62x: ENET : A53 : TCP Throughput drop in iperf application running on FreeRTOS A53 core Ethernet 11.00.00

Known Issues

ID Head Line Module Reported in release Workaround
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC 08.03.00 No known workaround
EXT_SITMPUSW-73 OSPI_readDirect and OSPI_isPhyEnable do not correctly check if the PHY is enabled OSPI 08.03.00 No known workaround
EXT_SITMPUSW-77 Modify Read capture delay logic for Tap Mode OSPI 08.03.00 No known workaround
EXT_SITMPUSW-78 MMCSD Sysconfig provides options to configure PHY type MMCSD 08.03.00 No known workaround
EXT_SITMPUSW-85 Flash_eraseSector and Flash_norOspiEraseSector does not erases the mentioned sector. Flash 08.03.00 No known workaround
EXT_SITMPUSW-87 Sysconfig crashing when adding large number of GPIO pins GPIO 08.03.00 No known workaround
EXT_EP-12275 AM62x: ECC: SDL_WKUP_R5FSS0_PULSAR_UL_CPU0_ECC_AGGR aggregator is failing on M4F core SDL 10.01.00 No known workaround
EXT_EP-12276 ECC: Firewall related aggregator failures - ECC Aggregators SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR and SDL_SMS0_SMS_TIFS_ECC fail because of firewall access issues faced by SDL SDL 10.01.00 No known workaround
EXT_EP-12278 ECC Aggregator SMS0_SMS_HSM_ECC Aggr fails on AM62x. SDL 10.00.00 No known workaround
EXT_EP-12279 CSI RX ECC aggregators are failing on AM62P/AM62X SDL 09.01.00 No known workaround

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 PHY mode not supported for OSPI NAND SBL on DDR mode. It is supported for SDR mode only Bootloader
3 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader

Upgrade and Compatibility Information

Attention
When migrating from oldder version to 11.00.00, see Bootloader Migration Guidelines for more details

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.