| Feature | Module |
| Bad block management support for OSPI NAND | OSPI |
| A53 Drivers: ECAP, EPWM, EQEP, GPMC, Spinlock | Drivers |
| GPIO default value can be configured in sysconfig | GPIO |
| GPIO direction is set part of sysconfig generated code | GPIO |
| FreeRTOS FAT is now supported with FreeRTOS | File System |
| QoS support | QoS |
| Early PLL driver in TIFS init updated to follow recommended sequence to avoid PLL instability | TIFS |
| PM PLL and HSDIV programing in PLL init updated to remove steps violating the recommendation | DM |
| Update | Module |
| ATF Load Address is updated to 0X80000000 from 0x9e780000 | LinuxAppImageGen, QnxAppImagegen |
| Linux FDT is added in qnx app image and loaded at DDR 0x88000000 | QnxAppImagegen |
| make commands are added in boardcfg makefile to open k3-resource-part tool | BoardCfg |
| OSPI tuning optimizations to redue tuning time | OSPI |
| I2C driver updated for inclusinve API names | I2C |
| Bootloader powers off cores if image not present | SBL |
| FreeRTOS FAT will now work with FreeRTOS application as well | FAT FS |
| ID | Head Line | Module | Applicable Releases |
| SITSW-3920 | DDR Inline ECC example does not work in debug mode on AM62x | DDR | 09.01.00 onwards |
| SITSW-3945 | Issues with the OSPI NAND PHY tuning | OSPI | 09.00.00 onwards |
| SITSW-4229 | OSPI NAND performance reduction when phy tuning is skipped | OSPI | 09.02.00 onwards |
| SITSW-4271 | Update the FSS_CTRL register to support 128MB flash size by default. | OSPI | 09.01.00 onwards |
| SITSW-4282 | Skip tuning is not happenning for sbl stage2 as stage1 closes the drivers. | OSPI | 09.01.00 onwards |
| SITSW-4337 | Bootloader_socInitR5FAtcmBtcm function uses global ATCM address resulting in CBASS error | SBL | 08.06.00 onwards |
| SITSW-4345 | A53 core freq is limited to 1250MHz in bootloader | SBL | 08.06.00 onwards |
| SITSW-4417 | No checks on number blocks in a single MMCSD R/W transaction | MMCSD | 09.02.00 onwards |
| SITSW-4549 | OSPI Read delay using an older value | OSPI | 09.02.00 onwards |
| SITSW-4599 | SysConfig Updates to UART Clock Frequency fails to reflect in ti_drivers_config.c | UART | 08.04.00 onwards |
| SITSW-4611 | Generated tiboot3.bin in SBL examples are copy of GP images instead of HSFS | SBL | 08.06.00 onwards |
| SITSW-4612 | UART driver is initialized late in the sysconfig generated code | UART | 08.06.00 onwards |
| SITSW-4613 | Generation of Board Configuration Binary fails for HS-SE device type | SBL | 08.06.00 onwards |
| SITSW-4630 | Hwip_disable API not working properly on M4F | DPL | 08.06.00 onwards |
| SITSW-4647 | AM62X : PADCFG offset value is missing for B16 pin | Pinmux | 08.06.00 onwards |
| PROC_SDL-7823 | Setting trim value for non-Ping pong mode POKs accesses invalid offset | SDL | 09.02.00 onwards |
| SYSFW-7536 | Sending JTAG unlock certificate to TIFS using T32 JTAG fails | TIFS | 09.02.01 onwards |
| SYSFW-7474 | Write access from DMA initiators to RA GCFG region results in firewall exception | TIFS | 08.06.00 onwards |
| SYSFW-7485 | Update the PLL driver in TIFS boot flow to follow correct sequence | TIFS | 08.06.00 onwards |
| SYSFW-7463 | TISCI_MSG_GET_CLOCK always return Enabled for input clock | DM | 08.06.00 onwards |
| SYSFW-7486 | PM: Cleanup additional steps in pll init startup routine | DM | 08.06.00 onwards |
| ID | Head Line | Module | Reported in release | Workaround |
| MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 07.03.00 | Use bash for windows as part of git for windows or don't use -j option |
| SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 08.06.00 | None. |
| SITSW-4001 | On SK-AM62-SIP, SBL with ECC enabled does not boot linux, when the SDRAM index is set to 13 | DDR | 09.01.00 | None. |
| SYSFW-5992 | Unable to set exact pixel clock for OLDI LCD display / HDMI Pixel clock | DM | 08.05.00 | Avoid gving range for SET_CLOCK, use exact values for min, max and target |
| SYSFW-6369 | DM unable to enter deep sleep mode when booting in SBL flow | DM | 08.03.00 | None. |
| SYSFW-6432 | Set device API doesn't return Error when PD is in transition state | DM | 08.03.00 | None. |
| SYSFW-6426 | Ownership of a firewall region can be transferred to an invalid host | TIFS | 08.03.00 | None. |
| SYSFW-7559 | LPM: In MCU Only mode resume path the MCU_M4 LPSC is ON | DM | 10.00.00 | None. |
| SYSFW-7571 | LPM: Device IDs higher than 255 will not work with set device constraint | DM | 10.00.00 | None. |
| PROC_SDL-8404 | ECC is not supported for some instances. These are SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR | SDL | 10.00.00 | None. Support will be added in future release. |
| PROC_SDL-8139 | SDL ECC example application exits with failure on UC-2 | SDL | 10.00.00 | Update the MPU config for the example to make the register region as Strongly Ordered. The Example app will be fixed in future release. |
| PROC_SDL-8138 | VTM example app fails when built for freertos | SDL | 10.00.00 | Use the nortos example. Example will be fixed in future release. |
| PROC_SDL-8137 | PBIST example app fails when built for freertos | SDL | 10.00.00 | Use the nortos example. Freertos example will be fixed in future release. |
| PROC_SDL-8134 | POK example app fails when built for freertos | SDL | 10.00.00 | Use the nortos example. Freertos example will be fixed in future release. |