AM62x MCU+ SDK  10.00.00
SAFETY APP

Introduction

The example demonstrates the usage of RM, PM and TIFS safety checker APIs.

  • PM Safety Checker can be used to validate PSC/PLL configurations
  • RM Safety Checkers can be used to validate RM module configurations
  • TIFS Safety Checker can be used to verify the firewall configuration

Each of these configurations can be validated using the Golden Reference.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62x-sk, am62x-sk-lp
Example folder examples/safety/safety_app/

Steps to Run the Example

See Also

SAFETY_APP

Sample Output

Shown below is a sample output when the application is run

Get PSC configuration successful.
Get PLL configuration successful.
Get RM configuration successful.
Firewall open successful.
Get firewall configuration successful.
Verifying registers against golden reference...
No register mismatch with golden reference.
Firewall close successful.