AM62x MCU+ SDK  10.00.00
SBL OSPI NAND Linux Multistage

Note
The load address of resource table for R5 and M4 cores must be consistant with the address in the Linux dts file.

Introduction

This is a bootloader example, which shows an example of booting Linux on A53 core and RTOS/NORTOS applications on DM R5 and M4 cores.

The booting is done in 2 stages(2 bootloader applications).

  • The stage1 of the bootloader runs from the HSM RAM. It boots MCU M4 with RTOS/NORTOS application and initializes the DDR. Then it loads the stage2 of the bootloader to DDR and stats running it.
  • The stage2 of the bootloader boots Linux on A53 and then self loads DM firmware on the DM R5.

The SBL uses 6 appimages

  • A Linux appimage containing the Linux binaries (ATF, OPTEE, A53 SPL).
  • tiboot3.bin with SBL stage1, TIFS, BoardConfig
  • Appimage for SBL stage2
  • Appimage for MCU M4
  • Appimage for HSM M4
  • DM firmware appimage for DM R5

Refer SBL Booting Linux From OSPI for more details on the OSPI boot loader.

Refer Enabling DDR inline ECC enablig inline ECC

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62x-sk-lp
Example folder examples/drivers/boot/sbl_ospi_nand_linux_multistage

Steps to Run the Example

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
    Note
    Change DEVICE_TYPE to HS in ${SDK_INSTALL_PATH}/devconfig/devconfig.mak and then generate Linux Appimage for HS-SE device.

Create Linux Appimage

Note
Change DEVICE_TYPE to HS in ${SDK_INSTALL_PATH}/devconfig/devconfig.mak and then generate Linux Appimage for HS-SE device.
  • Create a Linux Appimage containing the Linux binaries (ATF, OPTEE, A53 SPL)
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen after setting the PSDK path in file config.mak
  • Refer Linux Appimage Generator Tool for more details

Create HSM Appimage

Note
Change DEVICE_TYPE to HS in ${SDK_INSTALL_PATH}/devconfig/devconfig.mak and then generate HSM Appimage for HS-SE device.
  • Create a HSM Appimage
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/HSMAppimageGen
  • Refer HSM Appimage Generator Tool for more details

Run the example

  • This example is the SBL which needs to be flashed on the EVM flash, along with sample application images for R5, M4 CPUs and Linux Appimage.
Note
For HS-SE device, use default_sbl_ospi_nand_linux_hs.cfg as the cfg file.
For HS-FS device, use default_sbl_ospi_nand_linux_hs_fs.cfg as the cfg file.
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg Linux echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62x-sk-lp/default_sbl_ospi_nand_linux.cfg
    
  • Make sure IPC rpmsg linux echo application is built before running the flash script. (see IPC RP Message Linux Echo)
Note
For IPC rpmsg linux echo, the resource table entity must be placed at the beginning of remoteproc memory section as mentoined in Linux dts file.
  • To flash to the EVM, refer to Flash an example application . Only when giving the flash config file, point to the default_sbl_ospi_nand_linux.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and Linux Appimage is already created, in Windows,
      cd C:/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62x-sk-lp/default_sbl_ospi_nand_linux.cfg
    
  • If Linux PC is used, assuming SDK is installed at ~/ti/mcu_plus_sdk
      cd ~/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62x-sk-lp/default_sbl_ospi_nand_linux.cfg
    
  • Boot the EVM in OSPI NAND boot mode.
Note
The above config file will flash till u-boot on the OSPI NAND bootmedia. U-Boot can load kernel from any bootmedia, refer to Processor SDK Linux user guide for more details.

See Also

Sample Output

After flashing and booting the EVM, you will see below output on the UART console (Complete log is not shown)

SYSFW Version 9.0.5--v09.00.05 (Kool Koala)
SYSFW revision 0x9
DMSC ABI revision 3.1

[BOOTLOADER_PROFILE] Boot Media       : FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 182 KB
[BOOTLOADER_PROFILE] Cores present    :
m4f0-0
r5f0-0
[BOOTLOADER PROFILE] System_init                      :      37270us
[BOOTLOADER PROFILE] Drivers_open                     :        207us
[BOOTLOADER PROFILE] Board_driversOpen                :         88us
[BOOTLOADER PROFILE] Sciclient Get Version            :       9925us
[BOOTLOADER PROFILE] App_waitForMcuPbist              :          5us
[BOOTLOADER PROFILE] App_waitForMcuLbist              :       7689us
[BOOTLOADER PROFILE] App_loadImages                   :       5520us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :      10788us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      71496us

Image loading done, switching to application ...
Starting MCU-m4f and 2nd stage bootloader

SYSFW Version 9.0.5--v09.00.05 (Kool Koala)
SYSFW revision 0x9
DMSC ABI revision 3.1

[BOOTLOADER_PROFILE] Boot Media       : FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 895 KB
[BOOTLOADER_PROFILE] Cores present    :
hsm-m4f0-0
r5f0-0
a530-0
[BOOTLOADER PROFILE] System_init                      :       2845us
[BOOTLOADER PROFILE] Drivers_open                     :        269us
[BOOTLOADER PROFILE] Board_driversOpen                :         89us
[BOOTLOADER PROFILE] Sciclient Get Version            :       9976us
[BOOTLOADER PROFILE] App_loadImages                   :       2427us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :      11338us
[BOOTLOADER PROFILE] App_loadLinuxImages              :      52860us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      79806us

Image loading done, switching to application ...
Starting linux and RTOS/Baremetal applications
NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE:  BL31: Built : 00:42:57, Jan 13 2023

U-Boot SPL 2023.04-ga3595f1e3e (Jun 15 2023 - 08:14:46 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
Trying to boot from SPINAND


U-Boot 2023.04-ga3595f1e3e (Jun 15 2023 - 08:14:46 +0000)

SoC:   AM62X SR1.0 HS-FS
Model: Texas Instruments AM62x LP SK
EEPROM not available at 80, trying to read at 81
Board: AM62-LP-SKEVM rev E1
DRAM:  2 GiB



.
.
.
.
.
.


_____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
            |___|                    |___|

Arago Project am62xx-lp-evm -

Arago 2023.04 am62xx-lp-evm -

am62xx-lp-evm login: