AM62x MCU+ SDK  10.00.00
IPC RP Message Echo

Introduction

This example shows usage of RP Message APIs to each multi-byte messages between different CPUs

In this example,

  • One "main" CPU, sends multi-byte messages to other "remote" CPUs using the RP Message APIs
  • The "remote" CPUs, then echo back the same message to the main CPUs
  • Once all messages are echoed the main CPU exits. The remote CPUs remain waiting to receive new messages.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
m4fss0-0 nortos
a53ss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Boards am62x-sk, am62x-sip-sk, am62x-sk-lp
Example folder examples/drivers/ipc/ipc_rpmsg_echo

Steps to Run the Example

Note
This is a system or multi-core project, so refer to system project build instructions for CCS project or makefiles when building the example.
  • When using CCS projects to build, import the system CCS project and build it using the CCS project menu (see Using SDK with CCS Projects). This will build all the dependant CPU projects as well
  • When using makefiles to build, build the system makefile using make command (see Using SDK with Makefiles). This will build all the dependant CPU makefiles as well.
  • Launch a CCS debug session and run the executables, see CCS Launch, Load and Run
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
  • Refer Flash an example application for flashing the application.
  • This is a multi-core example. Hence the executables should be loaded and run for all the above mentioned cores
  • The application has a sync mechanism at the start which waits for all cores to start before doing the test. Hence the cores can be loaded and run in any sequence.

See Also

IPC RPMessage

Sample Output

Shown below is a sample output when the application is run,

  • After this the following message will appear on the WAKEUP UART.
    [IPC RPMSG ECHO] Message exchange started by main core !!!
    [IPC RPMSG ECHO] All echoed messages received by main core from 2 remote cores !!!
    [IPC RPMSG ECHO] Messages sent to each core = 10
    [IPC RPMSG ECHO] Number of remote cores = 2
    [IPC RPMSG ECHO] Total execution time = 438 usecs
    [IPC RPMSG ECHO] One way message latency = 10950 nsec
    All tests have passed!!