![Logo](ti_logo.svg) |
AM62x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
43 #include <drivers/hw_include/soc_config.h>
44 #include <board/flash/flash_config.h>
47 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
49 #define CONFIG_FLASH_TYPE_SERIAL ((uint32_t)0x1)
50 #define CONFIG_FLASH_TYPE_PARALLEL ((uint32_t)0x2)
55 #define CONFIG_FLASH_TYPE_SERIAL_NOR (0x00U)
56 #define CONFIG_FLASH_TYPE_SERIAL_NAND (0x01U)
57 #define CONFIG_FLASH_TYPE_PARALLEL_NOR (0x02U)
58 #define CONFIG_FLASH_TYPE_PARALLEL_NAND (0x03U)
59 #define CONFIG_FLASH_TYPE_INVALID (0xFFU)
92 typedef struct Flash_DevConfig_s {
192 uint8_t *buf, uint32_t len) ;
208 uint8_t *buf, uint32_t len) ;
300 typedef struct Flash_Params_s {
310 typedef struct Flash_Fxns_s
327 typedef struct Flash_Attrs_s {
348 typedef struct Flash_Config_s
359 #if defined (DRV_VERSION_SERIAL_FLASH_V0)
360 #include <board/flash/ospi/flash_nor_ospi.h>
361 #include <board/flash/ospi/flash_nand_ospi.h>
364 #if defined (DRV_VERSION_SERIAL_FLASH_V1)
365 #include <board/flash/qspi/flash_nor_qspi.h>
368 #if defined (DRV_VERSION_PARALLEL_FLASH_V0)
369 #include <board/flash/gpmc/flash_nand_gpmc.h>
uint8_t cmdPageLoadCyc1
Definition: flash.h:107
uint32_t flashType
Definition: flash.h:329
uint8_t cmdPageProgCyc1
Definition: flash.h:112
void Flash_close(Flash_Handle handle)
Close flash driver.
uint8_t cmdReadStatus
Definition: flash.h:116
SemaphoreP_Object lockSem
Definition: flash.h:354
uint32_t xspiRdsrDummy
Definition: flash.h:128
Flash_Attrs * attrs
Definition: flash.h:350
uint32_t flashSize
Definition: flash.h:334
uint32_t progStatusReg
Definition: flash.h:136
Flash_OpenFxn openFxn
Definition: flash.h:312
int32_t(* Flash_DisablePhyPipelineFxn)(Flash_Config *config)
Driver implementation to disable PHY pipeline mode in Flash.
Definition: flash.h:271
void Flash_deinit(void)
This function de-initializes the Flash module.
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:132
uint8_t cmdWrsr
Definition: flash.h:102
uint32_t blockCount
Definition: flash.h:335
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:134
uint8_t cmdExtType
Definition: flash.h:94
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:176
uint8_t cmdWren
Definition: flash.h:100
Flash_DevConfig * devConfig
Definition: flash.h:352
uint32_t driverInstance
Definition: flash.h:333
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:349
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
uint8_t cmdPageProg
Definition: flash.h:104
uint32_t srWipReg
Definition: flash.h:125
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:122
uint8_t cmdRdsr
Definition: flash.h:101
uint32_t xspiWipReg
Definition: flash.h:126
uint8_t cmdPageProgCyc2
Definition: flash.h:113
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:317
uint32_t flashBusyTimeout
Definition: flash.h:130
uint32_t sectorSize
Definition: flash.h:340
Flash_Fxns * fxns
Definition: flash.h:351
uint32_t pageSize
Definition: flash.h:338
uint8_t addrByteSupport
Definition: flash.h:97
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:191
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:327
char * flashName
Definition: flash.h:330
uint8_t cmdRandomReadCyc2
Definition: flash.h:110
uint32_t xspiWipBit
Definition: flash.h:127
Flash_EraseFxn eraseFxn
Definition: flash.h:316
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:311
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:221
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t fourByteAddrEnSeq
Definition: flash.h:99
uint8_t srWip
Definition: flash.h:105
uint8_t srWel
Definition: flash.h:120
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:80
uint8_t resetType
Definition: flash.h:121
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:207
Flash_CloseFxn closeFxn
Definition: flash.h:313
uint8_t cmdPageLoadCyc2
Definition: flash.h:108
uint32_t flashWriteTimeout
Definition: flash.h:129
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:247
uint32_t pageCount
Definition: flash.h:337
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:85
uint32_t spareAreaSize
Definition: flash.h:341
uint8_t pageRowAddrCyc
Definition: flash.h:115
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:292
int32_t(* Flash_EnablePhyPipelineFxn)(Flash_Config *config)
Driver implementation to enable PHY pipeline mode in Flash.
Definition: flash.h:259
Flash_EnablePhyPipelineFxn enablePhyPipelineFxn
Definition: flash.h:319
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:123
uint32_t blockSize
Definition: flash.h:336
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:133
int32_t Flash_disablePhyPipeline(Flash_Handle handle)
Disable PHY mode in flash.
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
uint32_t xspiEraseStatusReg
Definition: flash.h:139
int32_t Flash_enablePhyPipeline(Flash_Handle handle)
Enables PHY mode in flash.
uint8_t srWriteProtectMask
Definition: flash.h:143
Flash_DisablePhyPipelineFxn disablePhyPipelineFxn
Definition: flash.h:320
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:331
Flash_ReadFxn readFxn
Definition: flash.h:314
uint8_t enable4BAddr
Definition: flash.h:96
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:234
Flash_WriteFxn writeFxn
Definition: flash.h:315
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:164
uint8_t cmdReset
Definition: flash.h:117
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t cmdRandomInput
Definition: flash.h:111
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
uint8_t cmdRandomReadCyc1
Definition: flash.h:109
void Flash_init(void)
This function initializes the Flash module.
uint8_t byteOrder
Definition: flash.h:95
uint8_t srWriteProtectReg
Definition: flash.h:142
uint32_t manufacturerId
Definition: flash.h:332
uint8_t cmdPageLoad
Definition: flash.h:103
Flash_ResetFxn resetFxn
Definition: flash.h:318
uint8_t pageColAddrCyc
Definition: flash.h:114
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint8_t srEraseStatus
Definition: flash.h:141
uint32_t eraseStatusReg
Definition: flash.h:138
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:283
uint32_t sectorCount
Definition: flash.h:339
uint32_t xspiProgStatusReg
Definition: flash.h:137
Parameters passed during Flash_open()
Definition: flash.h:300
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:75
uint8_t srProgStatus
Definition: flash.h:140
uint32_t Flash_getFlashInterfaceIndex(uint32_t flashType)
Return flash index based on type of flash.
Flash_quirksFxn quirksFxn
Definition: flash.h:302
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:303
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:92
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
void * object
Definition: flash.h:353