| Feature | Module |
| FreeRTOS support for A53 is added (Single Core) | FreeRTOS, DPL |
| A53 Drivers: EMMC, GPIO, I2C, IPC, MCAN, McASP, McSPI, OSPI, SCI Client, SD, UART, UDMA, WDT | Drivers |
| SBL booting FreeRTOS on A53: EMMC, OSPI, SD, UART | Bootloader |
| ID | Head Line | Module | Applicable Releases |
| SITSW-4243 | Enabling DM firmware log causing the DM to go to abort | DM | 09.02.00 onwards |
| SITSW-4282 | Skip tunning is not happenig for SBL stage2 as stage1 is closing the OSPI driver | SBL | 09.02.00 onwards |
| SITSW-4337 | Bootloader_socInitR5FAtcmBtcm function uses global ATCM address resulting in CBASS error | SBL | 08.04.00 onwards |
| SITSW-4345 | A53 core freq is limited to 1250MHz in bootloader | SBL | 08.04.00 onwards |
| SITSW-4499 | TISCI_MSG_KEY_WRITER message is not part of secure context in SCI client | DM | 09.02.00 onwards |
| PROC_SDL-7266 | Main ESM events are being disabled instead of WKUP ESM for R5F core in SDL_POK_Thres_config_seq file | SDL | 09.02.01 onwards |
| SYSFW-6831 | DM self_reset operation stuck in abort_self_reset sometimes | DM | 08.04.00 onwards |
| SYSFW-7183 | Warm reset after system LPM entry/exit results in u-boot/DM hang | DM | 09.02.00 onwards |
| SYSFW-7251 | Enabling DM UART traces in boardcfg causes abort in DeepSleep resume path | DM | 09.02.00 onwards |
| SYSFW-7315 | Extra bypass step in boot time pll init routine | DM | 09.02.00 onwards |
| SYSFW-7327 | DM self reset goes to abort with logs enabled in SBL flow | DM | 09.02.00 onwards |
| SYSFW-7370 | pm init functions are missing proper return values | DM | 09.02.00 onwards |
| SYSFW-7375 | Firewall Exception during devices_init function in DM | DM | 09.02.00 onwards |
| SYSFW-7040 | JTAG unlock issue on MCU-M4 on AM62x HS-SE | DM | 08.06.00 onwards |
| ID | Head Line | Module | Reported in release | Workaround |
| MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 07.03.00 | Use bash for windows as part of git for windows or don't use -j option |
| SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 08.06.00 | None. |
| SITSW-4001 | On SK-AM62-SIP, SBL with ECC enabled does not boot linux, when the SDRAM index is set to 13 | DDR | 09.01.00 | None. |
| PROC_SDL-6300 | ECC is not supported for some instances when SDL is executed from M4F. These are SDL_ECC_AGGR0_SAM62_SEC_ECC_AGGR, SDL_ICSSM0_ICSS_M_CORE_BORG_ECC_AGGR, SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR, SDL_PSRAMECC_16K0_PSRAM16KX32E_ECC_AGGR, SDL_PSRAMECC0_PSRAM256X32E_ECC_AGGR. | SDL | 09.00.00 | None. |
| SYSFW-5992 | Unable to set exact pixel clock for OLDI LCD display / HDMI Pixel clock | DM | 08.05.00 | Avoid gving range for SET_CLOCK, use exact values for min, max and target |
| SYSFW-6369 | DM unable to enter deep sleep mode when booting in SBL flow | DM | 08.03.00 | None. |
| SYSFW-6432 | Set device API doesn't return Error when PD is in transition state | DM | 08.03.00 | None. |
| SYSFW-6426 | Ownership of a firewall region can be transferred to an invalid host | TIFS | 08.03.00 | None. |