Introduction
This example demonstrates the usage of the SDL ECC on R5F TCM module. The example shows how to setup and use the ECC Safety Diagnostic operation. Shows the generation of SEC and DED error on R5F TCM.
- Note
- DM swaps ATCM and BTCM addresses. ATCM starts at 0x41010000 and BTCM starts at 0x0.
Use Cases
| Use Case | Description |
| UC-1 | Double bit error injection. |
| UC-2 | Single bit error injection. |
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am62x-sk |
| Example folder | examples/sdl/ecc_tcm/ |
Steps to Run the Example
See Also
ECC
Sample Output
Shown below is a sample output when the application is run,
ECC TCM Example Application
ECC_Example_init: Init MAIN ESM complete
ECC_Example_init: Init WKUP ESM complete
AGGR ECC Init complete
ECC Safety Example tests: starting
B0TCM0 Bank0 Double bit error self test: starting
B0TCM0 Bank0 Double bit error self test: pErrMem 0x00000000 fixed location once test complete
Waiting for ESM Interrupt
UC-1: Got High priority ESM Interrupt
B0TCM0 Bank0 Single bit error inject test: starting
B0TCM0 Bank0 Single bit error inject test: at pErrMem 0x00000000: fixed location once test complete
Waiting for ESM Interrupt
UC-2: Got Low priority ESM Interrupt
ECC Safety Example tests: success
ECC UC-1 and UC-2 Test
All tests have passed.