AM62x MCU+ SDK  09.02.01
SBL SD

Introduction

This bootloader does SOC initializations and attempts to boot MCU M4 image by the name "app", DM R5 image by the name "dm", A53 image by the name "app_a53" present in the first FAT partition found in the connected SD card. The file can be copied to the SD card by connecting it to the host PC using a card reader. Make sure that the images are named without any file extension. If the card is new, make sure that it is formatted with FAT32/16.

If the appimage files are found at the location, the SBL reads the files into a buffer, parses it. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am62x-sk, am62x-sip-sk, am62x-sk-lp
Example folder examples/drivers/boot/sbl_sd

Steps to Run the Example

Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from an SD card unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Refer to the page Basic steps to flash files to flash this bootloader along with the application to boot.

See Also

BOOTLOADER

Sample Output

SYSFW Firmware Version 9.2.7--v09.02.07 (Kool Koala)
SYSFW Firmware revision 0x9
SYSFW ABI revision 3.1
[BOOTLOADER_PROFILE] Boot Media : SD Card
[BOOTLOADER_PROFILE] Boot Image Size : 198 KB
[BOOTLOADER_PROFILE] Cores present :
m4f0-0
r5f0-0
a530-0
[BOOTLOADER PROFILE] System_init : 33665us
[BOOTLOADER PROFILE] Board_init : 0us
[BOOTLOADER PROFILE] Drivers_open : 108146us
[BOOTLOADER PROFILE] Board_driversOpen : 0us
[BOOTLOADER PROFILE] File read from SD card : 10341us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_M4FSS0_0) : 152950us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_R5FSS0_0) : 141854us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_A53SS0_0) : 138552us
[BOOTLOADER PROFILE] SBL End : 150us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 585663us
Image loading done, switching to application ...
[IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
All tests have passed!!
SYSFW Firmware Version 9.2.7--v09.02.07 (Kool Koala)
SYSFW Firmware revision 0x9
SYSFW ABI revision 3.1
[BOOTLOADER_PROFILE] Boot Media : SD Card
[BOOTLOADER_PROFILE] Boot Image Size : 198 KB
[BOOTLOADER_PROFILE] Cores present :
m4f0-0
r5f0-0
a530-0
[BOOTLOADER PROFILE] System_init : 33597us
[BOOTLOADER PROFILE] Board_init : 0us
[BOOTLOADER PROFILE] Drivers_open : 108073us
[BOOTLOADER PROFILE] Board_driversOpen : 0us
[BOOTLOADER PROFILE] File read from SD card : 10335us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_M4FSS0_0) : 152960us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_R5FSS0_0) : 162888us
[BOOTLOADER PROFILE] App_loadImages(CSL_CORE_ID_A53SS0_0) : 159556us
[BOOTLOADER PROFILE] SBL End : 150us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 627564us
Image loading done, switching to application ...
[IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
All tests have passed!!