![Logo](ti_logo.svg) |
AM62x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
51 #include <sdl/pok/v1/sdl_ip_pok.h>
89 typedef struct SDL_Pok_Static_Reg_read{
Header file containing various enumerations, structure definitions and function declarations for the ...
bool porBGapOK
Definition: pok/v1/sdl_pok.h:102
uint8_t hystCtrl
Definition: pok/v1/sdl_pok.h:90
int8_t SDL_PRG_Inst
Definition: sdl_soc_pok.h:104
POK Configuration structure.
Definition: sdl_pok_def.h:418
int32_t SDL_POK_getStaticRegisters(SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
POK Function to get the Static Registers. This function reads the values of the static registers such...
POK Static Registers structure.
Definition: pok/v1/sdl_pok.h:89
This file contains the SDL DPL API's.
uint8_t hystCtrlOV
Definition: pok/v1/sdl_pok.h:92
uint8_t trimOV
Definition: pok/v1/sdl_pok.h:98
int32_t SDL_POK_verifyConfig(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK Function to verify the written configuration. This function checks the provided config against th...
uint8_t trim
Definition: pok/v1/sdl_pok.h:96
uint8_t voltDetMode
Definition: pok/v1/sdl_pok.h:94
uint8_t deglitch
Definition: pok/v1/sdl_pok.h:100
uint8_t porModuleStatus
Definition: pok/v1/sdl_pok.h:104
int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable)
POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version o...
int32_t SDL_POK_init(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK module configuration API.
int8_t SDL_POK_Inst
Definition: sdl_soc_pok.h:75