![Logo](ti_logo.svg) |
AM62x MCU+ SDK
09.01.00
|
|
Go to the documentation of this file.
53 #ifndef TISCI_DSMEK_H_
54 #define TISCI_DSMEK_H_
66 #define SA2UL_DSMEK_KEY_LEN (32U)
71 #define KDF_LABEL_AND_CONTEXT_LEN_MAX 41U
struct tisci_header hdr
Definition: tisci_dsmek.h:107
struct tisci_header hdr
Definition: tisci_dsmek.h:97
#define KDF_LABEL_AND_CONTEXT_LEN_MAX
key derivation label and context length
Definition: tisci_dsmek.h:71
struct tisci_msg_sa2ul_set_dsmek_req __attribute__((__packed__))
#define SA2UL_DSMEK_KEY_LEN
This file contains:
Definition: tisci_dsmek.h:66
TISCI Response for setting DSMEK in SA2UL registers.
Definition: tisci_dsmek.h:96
TISCI Request for setting DSMEK in SA2UL registers.
Definition: tisci_dsmek.h:84
TISCI Request for releasing DSMEK.
Definition: tisci_dsmek.h:106
TISCI Request for getting DSMEK via TISCI.
Definition: tisci_dsmek.h:130
uint8_t sa2ul_instance
Definition: tisci_dsmek.h:132
uint8_t kdf_label_and_context[KDF_LABEL_AND_CONTEXT_LEN_MAX]
Definition: tisci_dsmek.h:135
TISCI Response for Releasing DSMEK.
Definition: tisci_dsmek.h:115
TISCI Response for requesting DSMEK.
Definition: tisci_dsmek.h:143
uint8_t kdf_context_len
Definition: tisci_dsmek.h:88
uint8_t kdf_label_and_context[KDF_LABEL_AND_CONTEXT_LEN_MAX]
Definition: tisci_dsmek.h:89
uint8_t kdf_label_len
Definition: tisci_dsmek.h:87
struct tisci_header hdr
Definition: tisci_dsmek.h:116
struct tisci_header hdr
Definition: tisci_dsmek.h:85
struct tisci_header hdr
Definition: tisci_dsmek.h:144
uint8_t kdf_context_len
Definition: tisci_dsmek.h:134
uint8_t dsmek[SA2UL_DSMEK_KEY_LEN]
Definition: tisci_dsmek.h:145
uint8_t kdf_label_len
Definition: tisci_dsmek.h:133
uint8_t sa2ul_instance
Definition: tisci_dsmek.h:108
struct tisci_header hdr
Definition: tisci_dsmek.h:131
uint8_t sa2ul_instance
Definition: tisci_dsmek.h:86