|
AM62x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
53 #ifndef TISCI_PM_TISCI_DEVICE_H
54 #define TISCI_PM_TISCI_DEVICE_H
68 #define TISCI_MSG_FLAG_DEVICE_WAKE_ENABLED TISCI_BIT(8)
71 #define TISCI_MSG_FLAG_DEVICE_RESET_ISO TISCI_BIT(9)
80 #define TISCI_MSG_FLAG_DEVICE_EXCLUSIVE TISCI_BIT(10)
87 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_AUTO_OFF 0
90 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_RETENTION 1
93 #define TISCI_MSG_VALUE_DEVICE_SW_STATE_ON 2
99 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_OFF 0
105 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_ON 1
115 #define TISCI_MSG_VALUE_DEVICE_HW_STATE_TRANS 2
struct tisci_header hdr
Definition: tisci_pm_device.h:163
Empty response for TISCI_MSG_SET_DEVICE_RESETS.
Definition: tisci_pm_device.h:222
struct tisci_header hdr
Definition: tisci_pm_device.h:187
Request to get device based on id.
Definition: tisci_pm_device.h:162
uint32_t context_loss_count
Definition: tisci_pm_device.h:188
Empty response for TISCI_MSG_DEVICE_DROP_POWERUP_REF.
Definition: tisci_pm_device.h:251
uint8_t state
Definition: tisci_pm_device.h:139
struct tisci_header hdr
Definition: tisci_pm_device.h:136
struct tisci_header hdr
Definition: tisci_pm_device.h:223
Response to get device request.
Definition: tisci_pm_device.h:186
Empty response for TISCI_MSG_SET_DEVICE.
Definition: tisci_pm_device.h:150
Set the desired state of the device.
Definition: tisci_pm_device.h:135
struct tisci_header hdr
Definition: tisci_pm_device.h:252
Drop any remaining powerup device references.
Definition: tisci_pm_device.h:239
uint32_t reserved
Definition: tisci_pm_device.h:138
uint8_t programmed_state
Definition: tisci_pm_device.h:190
uint8_t current_state
Definition: tisci_pm_device.h:191
struct tisci_header hdr
Definition: tisci_pm_device.h:240
uint32_t id
Definition: tisci_pm_device.h:210
uint32_t resets
Definition: tisci_pm_device.h:211
struct tisci_header hdr
Definition: tisci_pm_device.h:209
uint32_t id
Definition: tisci_pm_device.h:137
uint32_t id
Definition: tisci_pm_device.h:164
struct tisci_msg_set_device_req __attribute__((__packed__))
uint32_t resets
Definition: tisci_pm_device.h:189
struct tisci_header hdr
Definition: tisci_pm_device.h:151
Set the desired state of the resets of a device.
Definition: tisci_pm_device.h:208