![Logo](ti_logo.svg) |
AM62x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
51 #if defined (SOC_AM62x)
52 #include <sdl/include/am62x/sdlr_soc_baseaddress.h>
53 #include <sdl/include/am62x/sdlr_mcu_ctrl_mmr.h>
56 #if defined (SOC_AM62Ax)
57 #include <sdl/include/am62ax/sdlr_soc_baseaddress.h>
58 #include <sdl/include/am62ax/sdlr_mcu_ctrl_mmr.h>
96 typedef struct SDL_Pok_Static_Reg_read{
Header file containing various enumerations, structure definitions and function declarations for the ...
bool porBGapOK
Definition: pok/v1/sdl_pok.h:109
int8_t SDL_POK_Inst
Definition: sdl_pok_def.h:135
uint8_t hystCtrl
Definition: pok/v1/sdl_pok.h:97
POK Configuration structure.
Definition: sdl_pok_def.h:425
int32_t SDL_POK_getStaticRegisters(SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
POK Function to get the Static Registers. This function reads the values of the static registers such...
int8_t SDL_PRG_Inst
Definition: sdl_pok_def.h:134
POK Static Registers structure.
Definition: pok/v1/sdl_pok.h:96
This file contains the SDL DPL API's.
uint8_t hystCtrlOV
Definition: pok/v1/sdl_pok.h:99
uint8_t trimOV
Definition: pok/v1/sdl_pok.h:105
int32_t SDL_POK_verifyConfig(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK Function to verify the written configuration. This function checks the provided config against th...
uint8_t trim
Definition: pok/v1/sdl_pok.h:103
uint8_t voltDetMode
Definition: pok/v1/sdl_pok.h:101
uint8_t deglitch
Definition: pok/v1/sdl_pok.h:107
uint8_t porModuleStatus
Definition: pok/v1/sdl_pok.h:111
int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable)
POK Function to enable or disable ping/pong mode for a specified PRG. Only supported for v1 version o...
int32_t SDL_POK_init(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK module configuration API.