![Logo](ti_logo.svg) |
AM62x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
43 #include <drivers/hw_include/soc_config.h>
44 #include <board/flash/flash_config.h>
46 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
48 #define CONFIG_FLASH_TYPE_SERIAL ((uint32_t)0x1)
49 #define CONFIG_FLASH_TYPE_PARALLEL ((uint32_t)0x2)
82 typedef struct Flash_DevConfig_s {
182 uint8_t *buf, uint32_t len) ;
198 uint8_t *buf, uint32_t len) ;
266 typedef struct Flash_Params_s {
276 typedef struct Flash_Fxns_s
291 typedef struct Flash_Attrs_s {
312 typedef struct Flash_Config_s
322 #if defined (DRV_VERSION_SERIAL_FLASH_V0)
323 #include <board/flash/ospi/flash_nor_ospi.h>
324 #include <board/flash/ospi/flash_nand_ospi.h>
327 #if defined (DRV_VERSION_SERIAL_FLASH_V1)
328 #include <board/flash/qspi/flash_nor_qspi.h>
331 #if defined (DRV_VERSION_PARALLEL_FLASH_V0)
332 #include <board/flash/gpmc/flash_nand_gpmc.h>
uint8_t cmdPageLoadCyc1
Definition: flash.h:97
uint32_t flashType
Definition: flash.h:293
uint8_t cmdPageProgCyc1
Definition: flash.h:102
void Flash_close(Flash_Handle handle)
Close flash driver.
uint8_t cmdReadStatus
Definition: flash.h:106
uint32_t xspiRdsrDummy
Definition: flash.h:118
Flash_Attrs * attrs
Definition: flash.h:314
uint32_t flashSize
Definition: flash.h:298
uint32_t progStatusReg
Definition: flash.h:126
Flash_OpenFxn openFxn
Definition: flash.h:278
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:122
uint8_t cmdWrsr
Definition: flash.h:92
uint32_t blockCount
Definition: flash.h:299
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:124
uint8_t cmdExtType
Definition: flash.h:84
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:166
uint8_t cmdWren
Definition: flash.h:90
Flash_DevConfig * devConfig
Definition: flash.h:316
uint32_t driverInstance
Definition: flash.h:297
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:313
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
uint8_t cmdPageProg
Definition: flash.h:94
uint32_t srWipReg
Definition: flash.h:115
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:112
uint8_t cmdRdsr
Definition: flash.h:91
uint32_t xspiWipReg
Definition: flash.h:116
uint8_t cmdPageProgCyc2
Definition: flash.h:103
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:283
uint32_t flashBusyTimeout
Definition: flash.h:120
uint32_t sectorSize
Definition: flash.h:304
Flash_Fxns * fxns
Definition: flash.h:315
uint32_t pageSize
Definition: flash.h:302
uint8_t addrByteSupport
Definition: flash.h:87
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:181
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:291
char * flashName
Definition: flash.h:294
uint8_t cmdRandomReadCyc2
Definition: flash.h:100
uint32_t xspiWipBit
Definition: flash.h:117
Flash_EraseFxn eraseFxn
Definition: flash.h:282
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:277
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:211
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t fourByteAddrEnSeq
Definition: flash.h:89
uint8_t srWip
Definition: flash.h:95
uint8_t srWel
Definition: flash.h:110
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:70
uint8_t resetType
Definition: flash.h:111
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:197
Flash_CloseFxn closeFxn
Definition: flash.h:279
uint8_t cmdPageLoadCyc2
Definition: flash.h:98
uint32_t flashWriteTimeout
Definition: flash.h:119
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:237
uint32_t pageCount
Definition: flash.h:301
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:75
uint32_t spareAreaSize
Definition: flash.h:305
uint8_t pageRowAddrCyc
Definition: flash.h:105
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:258
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:113
uint32_t blockSize
Definition: flash.h:300
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:123
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
uint32_t xspiEraseStatusReg
Definition: flash.h:129
uint8_t srWriteProtectMask
Definition: flash.h:133
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:295
Flash_ReadFxn readFxn
Definition: flash.h:280
uint8_t enable4BAddr
Definition: flash.h:86
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:224
Flash_WriteFxn writeFxn
Definition: flash.h:281
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:154
uint8_t cmdReset
Definition: flash.h:107
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t cmdRandomInput
Definition: flash.h:101
uint8_t cmdRandomReadCyc1
Definition: flash.h:99
uint8_t byteOrder
Definition: flash.h:85
uint8_t srWriteProtectReg
Definition: flash.h:132
uint32_t manufacturerId
Definition: flash.h:296
uint8_t cmdPageLoad
Definition: flash.h:93
Flash_ResetFxn resetFxn
Definition: flash.h:284
uint8_t pageColAddrCyc
Definition: flash.h:104
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint8_t srEraseStatus
Definition: flash.h:131
uint32_t eraseStatusReg
Definition: flash.h:128
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:249
uint32_t sectorCount
Definition: flash.h:303
uint32_t xspiProgStatusReg
Definition: flash.h:127
Parameters passed during Flash_open()
Definition: flash.h:266
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:65
uint8_t srProgStatus
Definition: flash.h:130
uint32_t Flash_getFlashInterfaceIndex(uint32_t flashType)
Return flash index based on type of flash.
Flash_quirksFxn quirksFxn
Definition: flash.h:268
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:269
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:82
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
void * object
Definition: flash.h:317