| SOC | Supported CPUs | EVM | Host PC |
|---|---|---|---|
| AM62x | M4F, R5F | AM62x SK EVM (referred to as am62x-sk in code), AM62x SK LP EVM (referred to as am62x-sk-lp in code) | Windows 10 64b or Ubuntu 18.04 64b |
| Feature | Module |
|---|---|
| DMA Support on OSPI NOR and OSPI NAND SBLs | Bootloader |
| MCU Domain reset isolation example | Safety Examples |
| OTP Writer example | OTP |
| HS-FS and HS-SE support | Bootloader |
| Device Manager is available as source in MCU+SDK | Device Manager |
| I2C, SPI, GPIO, MCAN, IPC, UART drivers and examples for DM R5 (WKUP_R5) | I2C, SPI, GPIO, MCAN, IPC, UART |
| Support for ESM, MCRC, RTI, DCC, VTM, STOG, PBIST, MTOG, POK, ECC modules are added as part of SDL | SDL |
| Tools | Supported CPUs | Version |
|---|---|---|
| Code Composer Studio | M4F, R5F | 12.3.0 |
| SysConfig | M4F, R5F | 1.16.1, build 2960 |
| TI ARM CLANG | M4F, R5F | 2.1.3.LTS |
| FreeRTOS Kernel | M4F, R5F | 10.4.3 |
| OS | Supported CPUs | SysConfig Support |
|---|---|---|
| FreeRTOS Kernel | M4F, R5F | NA |
| FreeRTOS POSIX | M4F | NA |
| NO RTOS | M4F, R5F | NA |
| Module | Supported CPUs | SysConfig Support | OS support |
|---|---|---|---|
| Address Translate | M4F, R5F | YES | FreeRTOS, NORTOS |
| Cache | R5F | YES | FreeRTOS, NORTOS |
| Clock | M4F, R5F | YES | FreeRTOS, NORTOS |
| CycleCounter | M4F, R5F | NA | FreeRTOS, NORTOS |
| Debug | M4F, R5F | YES | FreeRTOS, NORTOS |
| Heap | M4F, R5F | NA | FreeRTOS, NORTOS |
| Hwi | M4F, R5F | YES | FreeRTOS, NORTOS |
| MPU | M4F, R5F | YES | FreeRTOS, NORTOS |
| Semaphore | M4F, R5F | NA | FreeRTOS, NORTOS |
| Task | M4F, R5F | NA | FreeRTOS |
| Timer | M4F, R5F | YES | FreeRTOS, NORTOS |
| SBL Mode | Supported CPUs | SysConfig Support | PHY Support | DMA Support | OS support |
|---|---|---|---|---|---|
| OSPI NOR | R5F | YES | Yes | Yes | NORTOS |
| OSPI NAND | R5F | YES | No | Yes | NORTOS |
| EMMC | R5F | YES | NA | NA | NORTOS |
| UART | R5F | YES | NA | No | NORTOS |
| Peripheral | Domain | Supported CPUs | SysConfig Support |
|---|---|---|---|
| DDR | Main | R5F | YES |
| GPIO | MCU | M4F, R5F | YES |
| Main | M4F, R5F | YES | |
| I2C | Main | M4F, R5F | YES |
| MCU | M4F, R5F | YES | |
| Wakeup | M4F, R5F | YES | |
| IPC | Main | M4F, R5F | YES |
| MCAN | Main | R5F | YES |
| MCU | M4F | YES | |
| MCSPI | Main | M4F, R5F | YES |
| MCU | M4F, R5F | YES | |
| Pinmux | Main | M4F, R5F | YES |
| MCU | M4F, R5F | YES | |
| Wakeup | M4F, R5F | YES | |
| SOC | NA | M4F, R5F | YES |
| SCIClient | NA | M4F, R5F | YES |
| UART | Main | M4F, R5F | YES |
| MCU | M4F, R5F | YES | |
| Wakeup | R5F | YES |
| Peripheral | Supported CPUs | SysConfig Support |
|---|---|---|
| Flash | R5F | YES |
| SDL Module | Supported CPUs | SysConfig Support |
|---|---|---|
| ESM | M4F, R5F | NO |
| MCRC | M4F, R5F | NO |
| RTI | M4F, R5F | NO |
| DCC | M4F, R5F | NO |
| VTM | M4F, R5F | NO |
| STOG | M4F, R5F | NO |
| PBIST | M4F, R5F | NO |
| MTOG | M4F | NO |
| POK | M4F, R5F | NO |
| ECC | M4F, R5F | NO |
NA
| ID | Head Line | Module | Reported in release | Workaround |
|---|---|---|---|---|
| MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 7.3.0 | Use bash for windows as part of git for windows or don't use -j option |
| SITSW-2057 | SBL is not disabling the interrupts before self loading the DM firmware and jump to DM firmware | SBL | 8.6.0 | Disable all the interrupt before jumping to DM firmware. |
| SITSW-1766 | Utility out2rprc not generating correct appimage if data sections have different load and run addresses | Tools | 8.6.0 | None. |
| SITSW-1962 | MPU configuration reset is not done before loading the new configuration. | DPL | 8.6.0 | None. |
| SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 8.6.0 | None. |
| PROC_SDL-5743 | ECC is not supported for 2 instances. These are SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR and SDL_MCU_ECC_AGGR0_SAM62_MCU_ECC_AGGR | SDL | 8.6.0 | None. Support will be added in future release. |
| PROC_SDL-5742 | PBIST is not supported on Main instance from M4F. | SDL | 8.6.0 | None. Support will be added in future release. |
| PROC_SDL-5753 | ECC example is not supported on R5F. | SDL | 8.6.0 | Refer ECC example on M4F. |
| S.No | Head Line | Module |
|---|---|---|
| 1 | The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK | NA |
| 2 | PHY mode not supported for OSPI NAND SBL | Bootloader |