This example can be used to trigger firewall exceptions. The core running this example waits for the user to enter one of the following two characters:
Consequently, a firewall exception takes place. This example is used with the Firewall Exception Log Example example to trigger firewall exceptions, the latter one responds to exception events as and when they take place.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am62x-sk, am62x-sk-lp |
Example folder | examples/security/fwl_exception_trigger |
Shown below is a sample output when the application is run,