![Logo](ti_logo.svg) |
AM62x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
80 #define SDL_MTOG_FORCE_KEY ((uint32_t) 0x95U)
SDL_MTOGVal timeOut
Definition: sdl_mtog.h:97
Definition: sdl_mtog.h:95
int32_t SDL_MTOG_verifyConfig(SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
Verifying written configuration with Master TOG module.
int32_t SDL_MTOG_reset(SDL_MTOG_Inst instance)
Reset the timeout functionality.
int32_t SDL_MTOG_forceTimeout(SDL_MTOG_Inst instance)
Force a timeout.
int32_t SDL_MTOG_init(SDL_MTOG_Inst instance, const SDL_MTOG_config *pConfig)
Initialize Master TOG module with respect of instance.
Master TOG Static Registers.
Definition: sdl_mtog.h:89
int32_t SDL_MTOG_getStaticRegisters(SDL_MTOG_Inst instance, SDL_MTOG_staticRegs *pStaticRegs)
Readback Static configuration register.
int32_t SDL_MTOG_stop(SDL_MTOG_Inst instance)
Stop the timeout function.
uint32_t mtogCtrlRegister
Definition: sdl_mtog.h:91
uint32_t SDL_MTOGVal
Definition: sdl_ip_mtog.h:59
int32_t SDL_MTOG_start(SDL_MTOG_Inst instance)
Start the timeout function.
uint8_t SDL_MTOG_Inst
MTOG Instance supported.
Definition: sdl_soc_mtog.h:59