![Logo](ti_logo.svg) |
AM62x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
50 #include <sdl/pok/v1/sdl_ip_pok.h>
51 #include <sdl/esm/sdl_ip_esm.h>
54 #if defined (SOC_AM62x)
55 #include <sdl/include/am62x/sdlr_soc_baseaddress.h>
56 #include <sdl/include/am62x/sdlr_mcu_ctrl_mmr.h>
int8_t SDL_POK_Inst
Definition: sdl_pok_def.h:130
POK Configuration structure.
Definition: sdl_pok_def.h:420
int32_t SDL_POK_getStaticRegisters(SDL_POK_Inst instance, SDL_POK_staticRegs *pStaticRegs)
POK Function to get the Static Registers. This function reads the values of the static registers such...
int8_t SDL_PRG_Inst
Definition: sdl_pok_def.h:129
This file contains the SDL DPL API's.
int32_t SDL_POK_verifyConfig(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK Function to verify the written configuration. This function checks the provided config against th...
int32_t SDL_POK_enablePP(SDL_PRG_Inst instance, bool enable)
POK Static Registers structure.
int32_t SDL_POK_init(SDL_POK_Inst instance, SDL_POK_config *pConfig)
POK module configuration API.