![Logo](ti_logo.svg) |
AM62x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
43 #include <drivers/hw_include/soc_config.h>
44 #include <board/flash/flash_config.h>
46 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
79 typedef struct Flash_DevConfig_s {
171 uint8_t *buf, uint32_t len) ;
187 uint8_t *buf, uint32_t len) ;
255 typedef struct Flash_Params_s {
265 typedef struct Flash_Fxns_s
280 typedef struct Flash_Attrs_s {
300 typedef struct Flash_Config_s
310 #if defined (DRV_VERSION_FLASH_V0)
311 #include <board/flash/ospi/flash_nor_ospi.h>
314 #if defined (DRV_VERSION_FLASH_V1)
315 #include <board/flash/qspi/flash_nor_qspi.h>
318 #if defined (DRV_VERSION_FLASH_V2)
319 #include <board/flash/ospi/flash_nand_ospi.h>
uint8_t cmdPageLoadCyc1
Definition: flash.h:94
uint32_t flashType
Definition: flash.h:282
void Flash_close(Flash_Handle handle)
Close flash driver.
uint32_t xspiRdsrDummy
Definition: flash.h:107
Flash_Attrs * attrs
Definition: flash.h:302
uint32_t flashSize
Definition: flash.h:287
uint32_t progStatusReg
Definition: flash.h:115
Flash_OpenFxn openFxn
Definition: flash.h:267
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:111
uint8_t cmdWrsr
Definition: flash.h:89
uint32_t blockCount
Definition: flash.h:288
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:113
uint8_t cmdExtType
Definition: flash.h:81
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:155
uint8_t cmdWren
Definition: flash.h:87
Flash_DevConfig * devConfig
Definition: flash.h:304
uint32_t driverInstance
Definition: flash.h:286
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:301
uint8_t pageLoadColAddrCyc
Definition: flash.h:96
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
uint8_t cmdPageProg
Definition: flash.h:91
uint32_t srWipReg
Definition: flash.h:104
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:101
uint8_t cmdRdsr
Definition: flash.h:88
uint32_t xspiWipReg
Definition: flash.h:105
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:272
uint32_t flashBusyTimeout
Definition: flash.h:109
uint32_t sectorSize
Definition: flash.h:293
Flash_Fxns * fxns
Definition: flash.h:303
uint32_t pageSize
Definition: flash.h:291
uint8_t addrByteSupport
Definition: flash.h:84
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:170
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:280
char * flashName
Definition: flash.h:283
uint32_t xspiWipBit
Definition: flash.h:106
Flash_EraseFxn eraseFxn
Definition: flash.h:271
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:266
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:200
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t fourByteAddrEnSeq
Definition: flash.h:86
uint8_t srWip
Definition: flash.h:92
uint8_t srWel
Definition: flash.h:99
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:67
uint8_t resetType
Definition: flash.h:100
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:186
Flash_CloseFxn closeFxn
Definition: flash.h:268
uint8_t cmdPageLoadCyc2
Definition: flash.h:95
uint8_t pageLoadRowAddrCyc
Definition: flash.h:97
uint32_t flashWriteTimeout
Definition: flash.h:108
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:226
uint32_t pageCount
Definition: flash.h:290
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:72
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:247
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:102
uint32_t blockSize
Definition: flash.h:289
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:112
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
uint32_t xspiEraseStatusReg
Definition: flash.h:118
uint8_t srWriteProtectMask
Definition: flash.h:122
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:284
Flash_ReadFxn readFxn
Definition: flash.h:269
uint8_t enable4BAddr
Definition: flash.h:83
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:213
Flash_WriteFxn writeFxn
Definition: flash.h:270
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:143
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t byteOrder
Definition: flash.h:82
uint8_t srWriteProtectReg
Definition: flash.h:121
uint32_t manufacturerId
Definition: flash.h:285
uint8_t cmdPageLoad
Definition: flash.h:90
Flash_ResetFxn resetFxn
Definition: flash.h:273
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint8_t srEraseStatus
Definition: flash.h:120
uint32_t eraseStatusReg
Definition: flash.h:117
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:238
uint32_t sectorCount
Definition: flash.h:292
uint32_t xspiProgStatusReg
Definition: flash.h:116
Parameters passed during Flash_open()
Definition: flash.h:255
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:62
uint8_t srProgStatus
Definition: flash.h:119
Flash_quirksFxn quirksFxn
Definition: flash.h:257
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:258
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:79
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
void * object
Definition: flash.h:305