makefile
inside the ${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/ folder.This section describes the various tools used in conjunction with System Controller Firmware (SYSFW)
Folder/Files | Description |
---|---|
${SDK_INSTALL_PATH}/tools/bin2c/ | |
bin2c.py | Tool to convert a binary file to a C array of hexadecimals |
${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/ | |
sysfw_boardcfg_validator.py | Python script which validates the boardcfg. Used internally in the boardcfg makefile |
SYSFW Board Config is a SOC specific configuration data regarding the various system attributes controlled by the SYSFW. These include resources, power and clock, security etc. This configuration is sent to SYSFW during boot time. The default configuration is stored in source/drivers/sciclient/sciclient_defaultBoardCfg/{SOC}/
To enable the SYSFW trace, change the #undef SYSFW_TRACE_ENABLE
to #define SYSFW_TRACE_ENABLE
on source/drivers/sciclient/sciclient_defaultBoardCfg/{SOC}/sciclient_defaultBoardcfg.c
. Then rebuild the boardcfg as explained in the above section.
The DM firmware log shall be available at the wakeup UART (/dev/ttyUSB2). Connect to the UART through minicom to see the logs.
The TIFS logs can be obtained from the TIFS memory address as per the system firmware documentation