| Feature | Module |
| DMA Support on OSPI NOR and OSPI NAND SBLs | Bootloader |
| MCU Domain reset isolation example | Safety Examples |
| OTP Writer example | OTP |
| HS-FS and HS-SE support | Bootloader |
| Device Manager is available as source in MCU+SDK | Device Manager |
| I2C, SPI, GPIO, MCAN, IPC, UART drivers and examples for DM R5 (WKUP_R5) | I2C, SPI, GPIO, MCAN, IPC, UART |
| Support for ESM, MCRC, RTI, DCC, VTM, STOG, PBIST, MTOG, POK, ECC modules are added as part of SDL | SDL |
| ID | Head Line | Module | Reported in release | Workaround |
| MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 7.3.0 | Use bash for windows as part of git for windows or don't use -j option |
| SITSW-2057 | SBL is not disabling the interrupts before self loading the DM firmware and jump to DM firmware | SBL | 8.6.0 | Disable all the interrupt before jumping to DM firmware. |
| SITSW-1766 | Utility out2rprc not generating correct appimage if data sections have different load and run addresses | Tools | 8.6.0 | None. |
| SITSW-1962 | MPU configuration reset is not done before loading the new configuration. | DPL | 8.6.0 | None. |
| SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 8.6.0 | None. |
| PROC_SDL-5670 | ECC is not supported for 12 instances. These are CSI_RX_IF_EDC_CTRL_0, ICB_RAMECC, ITE_RAMECC, LPI_RAMECC, comput cluster core0-3 and corepac, USB2SS_16FFC_USB2SS_CORE_AXI2VBUSM_MST_KSBUS_AXI2VBUSM_RDATA_BUFFER, USB2SS_16FFC_USB2SS_CORE_RAMS_MEM_CTRL_RA M0, AM62_MCU_CBASS_SCRP_32B_CLK4_SCR_AM62_MCU_CBASS_SCRP_32B_CLK4_SCR_EDC_CTRL_BUSECC_1, PSRAM16KX32E_PSRAM0_ECC, PSRAM256X32E_PSRAM0_ECC, USB2SS_16FFC_USB2SS_CORE_AXI2VBUSM_MST_KSB US_AXI2VBUSM_RDATA_BUFFER, USB2SS_16FFC_USB2SS_CORE_RAMS_MEM_CTRL_RA M0 | SDL | 8.6.0 | None. Support will be added in future release. |
| PROC_SDL-5671 | PBIST is not supported for some of the instances. From R5F, PBIST is not supported for MPU instance. From M4F, PBIST is not supported for MPU and MAIN instances. | SDL | 8.6.0 | None. Support will be added in future release. |