Using CCS projects
- When using CCS projects to build, make sure you have imported and built the CCS project of interest (see Using SDK with CCS Projects)
- Quick steps to import the "hello world example" CCS project are listed below
- In CCS, goto "Toolbar > View > Project Explorer"
- In the "Project Explorer" window, right click and select "Import > CCS Projects"
- Click "Browse" and goto the folder
${SDK_INSTALL_DIR}/examples/hello_world
- Select the project
hello_world_{board}_m4fss0-0_freertos_ti-arm-clang
- The project will be imported into the "Project Explorer"
- Right click on the project title and click "Build Project"
- This will build the project, now you can load and run it (see CCS Launch, Load and Run)
Using makefiles
- When using makefiles to build, make sure you have built the example of interest using makefiles (see Using SDK with Makefiles)
- Given below is the command to build the "hello world example". Note, use
make
in Linux
cd ${SDK_INSTALL_PATH}
gmake -s -C examples/hello_world/{board}/m4fss0-0_freertos/ti-arm-clang
Rebuilding libraries