- Note
- To see the exact sequence of steps in which boardcfg generation is done, see the
makefile
inside the ${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/ folder.
Introduction
This section describes the various tools used in conjunction with System Controller Firmware (SYSFW)
Tool requirements on host PC
- The tools mentioned are implemented using python and needs python version 3.x
- Refer to the page, Python3 , to install python and the required python packages on your PC.
Important files and folders
Folder/Files | Description |
${SDK_INSTALL_PATH}/tools/bin2c/ |
bin2c.py | Tool to convert a binary file to a C array of hexadecimals |
${SDK_INSTALL_PATH}/tools/sysfw/boardcfg/ |
sysfw_boardcfg_validator.py | Python script which validates the boardcfg. Used internally in the boardcfg makefile |
SYSFW Board Config Generation
SYSFW Board Config is a SOC specific configuration data regarding the various system attributes controlled by the SYSFW. These include resources, power and clock, security etc. This configuration is sent to SYSFW during boot time. The default configuration is stored in source/drivers/sciclient/sciclient_defaultBoardCfg/{SOC}/
- Resource Management BoardCfg - sciclient_defaultBoardCfg_rm.c
- Power Management BoardCfg - sciclient_defaultBoardCfg_pm.c
- Security BoardCfg - sciclient_defaultBoardCfg_security.c
- For sending it to SYSFW, these files are converted to hex arrays. We use the bin2c.py python script to do this. This is done internally in the boardcfg makefile. If we change the boardcfg in the above mentioned files, run the following command to generate the hex array header files
cd ${SDK_INSTALL_PATH}
gmake -s -C tools/sysfw/boardcfg SOC=am62x
cd ${SDK_INSTALL_PATH}
gmake -s -C tools/sysfw/boardcfg SOC=am62ax
- Once these header files are generated, rebuild the libraries by doing
cd ${SDK_INSTALL_PATH}
gmake -s libs
- After this, make sure to rebuild the secondary bootloader (SBL) applications. You can do this by
cd ${SDK_INSTALL_PATH}
gmake -s sbl