Introduction
- SBL booting Linux (see SBL OSPI Linux) is a secondary bootloader application that boots Linux on A53 core and RTOS/NORTOS application on R5, M4 cores.
- The bootloader makes use of 6 appimages
- A Linux appimage containing the Linux binaries (ATF, OPTEE, SPL).
- Appimage for SBL stage1
- Appimage for SBL stage2
- Appimage for MCU M4
- Appimage for HSM M4
- DM firmware appimage for DM R5
- The Linux appimage can be generated by using Linux Appimage Generator Tool
- The appimages will be flashed to the offset specified by SysCfg, the SBL parses the appimages from these locations, loads and run the cores.
Features Supported
- Boots R5, M4 cores and Linux on A53 from OSPI.
- SBL booting Linux can be used when early booting of R5 and M4 cores are required. When using uBoot to run R5 and M4 cores the application will start running on R5, M4 cores only after booting Linux
Features NOT Supported
- If SD card or other boot modes are required, user might need to switch to booting Linux using Linux uBoot.
Bootflow for SBL booting linux from OSPI
- Note
- The binaries for R5, M4 cores need not be in the linux root partition
(root/lib/firmware)
, when SBL is booting Linux.
- The bootflow for SBL booting Linux is as follows
Bootflow for SBL booting Linux
OSPI memory layout for SBL booting Linux from OSPI
- Note
- The flash address R5, M4 appimages and Linux appimages can be configured using Syscfg
0x0 +----------------------------+
| tiboot3.bin |
| (SBL stage1,TIFS,boardcfg) |
| |
0x80000 +----------------------------+
| SBL Stage2 |
| |
0x100000 +----------------------------+
| MCU M4 App Image |
| |
0x280000 +----------------------------+
| ospi.u-boot(4m) |
| |
0x680000 +----------------------------+
| ospi.env(128k) |
| |
0x6c0000 +----------------------------+
| ospi.env.backup(128k) |
| |
0x740000 +----------------------------+
| padding (768k) |
0x800000 +----------------------------+
| HSM App Image |
| |
0xA00000 +----------------------------+
| DM App Image |
| |
0xC00000 +----------------------------+
| Linux App Image |
| |
0x3fc0000 +----------------------------+
| ospi.phypattern (256k) |
| |
+----------------------------+
SD card Partitioning
- Note
- The default SD card image for AM62x-evm can be used to boot Linux using SBL
-
The tiboot3.bin, tispl.bin will not be used for booting Linux when using SBL booting Linux.
-
The R5 binaries in the root partition (eg :
root/lib/firmware/am62-main-r5f0_0-fw
) will not be used when SBL boots Linux and R5,M4 cores.
The default Linux SD card image for AM62x-evm has two partitons
- A FAT partition (boot) contatining
- tiboot3.bin
- tispl.bin
- u-boot.img
- uboot.env
- A ext4 partition (root) containing
- Linux Kernel image
- Linux DTB
- Linux file system
See Also