| Feature | Module |
|---|---|
| SPI driver support is added for M4F | SPI |
| OSPI NOR, OSPI NAND, EMMC, UART and NULL SBL support | Bootloader |
| SBL UART uniflash support | Bootloader |
| FreeRTOS task switch and posix demo examples added | FreeRTOS |
| Access to main domain GPIO, I2C, SPI and UART from MCU M4 added through sysconfig | GPIO, I2C, SPI, UART |
| SOC | Supported CPUs | EVM | Host PC |
|---|---|---|---|
| AM62x | M4F, R5F | AM62x SK EVM (referred to as am62x-sk in code), AM62x SK LP EVM (referred to as am62x-sk-lp in code) | Windows 10 64b or Ubuntu 18.04 64b |
| Tools | Supported CPUs | Version |
|---|---|---|
| Code Composer Studio | M4F, R5F | 12.0.0 |
| SysConfig | M4F, R5F | 1.13.0, build 2553 |
| TI ARM CLANG | M4F, R5F | 2.1.1.LTS |
| FreeRTOS Kernel | M4F | 10.4.3 |
| OS | Supported CPUs | SysConfig Support |
|---|---|---|
| FreeRTOS Kernel | M4F | NA |
| FreeRTOS POSIX | M4F | NA |
| NO RTOS | M4F | NA |
| Module | Supported CPUs | SysConfig Support | OS support |
|---|---|---|---|
| Address Translate | M4F | YES | FreeRTOS, NORTOS |
| Clock | M4F | YES | FreeRTOS, NORTOS |
| CycleCounter | M4F | NA | FreeRTOS, NORTOS |
| Debug | M4F | YES | FreeRTOS, NORTOS |
| Heap | M4F | NA | FreeRTOS, NORTOS |
| Hwi | M4F | YES | FreeRTOS, NORTOS |
| MPU | M4F | YES | FreeRTOS, NORTOS |
| Semaphore | M4F | NA | FreeRTOS, NORTOS |
| Task | M4F | NA | FreeRTOS |
| Timer | M4F | YES | FreeRTOS, NORTOS |
| SBL Mode | Supported CPUs | SysConfig Support | PHY Support | DMA Support | OS support |
|---|---|---|---|---|---|
| OSPI NOR | R5F | YES | Yes | No | NORTOS |
| OSPI NAND | R5F | YES | No | No | NORTOS |
| EMMC | R5F | YES | NA | NA | NORTOS |
| UART | R5F | YES | NA | No | NORTOS |
| Peripheral | Supported CPUs | SysConfig Support |
|---|---|---|
| DDR | R5F | YES |
| I2C | M4F | YES |
| IPC Rpmsg | M4F | YES |
| MCAN | M4F | YES |
| MCSPI | M4F | YES |
| Pinmux | R5F, M4F | YES |
| SOC | R5F, M4F | YES |
| Sciclient | M4F | YES |
| UART | M4F | YES |
| Peripheral | Supported CPUs | SysConfig Support |
|---|---|---|
| Flash | R5F | YES |
| ID | Head Line | Module | Reported in release | Workaround |
|---|---|---|---|---|
| SITSW-1628 | SBL EMMC not booting the app images of size more than 2MB | Bootloader | 8.4.0 | None |
| MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 7.3.0 | Use bash for windows as part of git for windows or don't use -j option |
| SITSW-1382 | MCU UART prints a single character of junk data on the first print after the power cycle of the EVM | MCU UART | 8.3.0 | None |
| S.No | Head Line | Module |
|---|---|---|
| 1 | The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK | NA |
| 2 | DMA not supported for OSPI NOR, UART SBLs | Bootloader |
| 3 | DMA, PHY mode not supported for OSPI NAND SBL | Bootloader |