|
AM62Px MCU+ SDK
12.00.00
|
|
Go to the documentation of this file.
78 #define CSL_DSS_VID_PIPE_TYPE_VID ((uint32_t) 0x0)
80 #define CSL_DSS_VID_PIPE_TYPE_VIDL ((uint32_t) 0x1)
91 #define CSL_DSS_COMM_REG_ID_0 ((uint32_t) 0x0U)
93 #define CSL_DSS_COMM_REG_ID_1 ((uint32_t) 0x1U)
95 #define CSL_DSS_COMM_REG_ID_MAX ((uint32_t) 0x2U)
106 #define CSL_DSS_VID_PIPE_ID_VID1 ((uint32_t) 0x0U)
108 #define CSL_DSS_VID_PIPE_ID_VIDL1 ((uint32_t) 0x1U)
110 #define CSL_DSS_VID_PIPE_ID_MAX ((uint32_t) 0x2U)
112 #define CSL_DSS_VID_PIPE_ID_INVALID ((uint32_t) 0xFFU)
123 #define CSL_DSS_OVERLAY_ID_1 ((uint32_t) 0x0U)
125 #define CSL_DSS_OVERLAY_ID_2 ((uint32_t) 0x1U)
127 #define CSL_DSS_OVERLAY_ID_MAX ((uint32_t) 0x2U)
138 #define CSL_DSS_VP_ID_1 ((uint32_t) 0x0U)
140 #define CSL_DSS_VP_ID_2 ((uint32_t) 0x1U)
142 #define CSL_DSS_VP_ID_MAX ((uint32_t) 0x2U)
153 #define CSL_DSS_VP_ID_1_MASK ((uint32_t) 0x1U)
155 #define CSL_DSS_VP_ID_2_MASK ((uint32_t) 0x2U)
166 #define CSL_DSS_CSC_RANGE_LIMITED ((uint32_t) 0x0U)
168 #define CSL_DSS_CSC_RANGE_FULL ((uint32_t) 0x1U)
170 #define CSL_DSS_CSC_RANGE_CUSTOM ((uint32_t) 0x2U)
181 #define CSL_DSS_SAFETY_CHK_FRAME_FREEZE_DETECT \
182 ((uint32_t) CSL_DSS_VID_SAFETY_ATTRIBUTES_CAPTUREMODE_VAL_FRAMEFREEZE)
184 #define CSL_DSS_SAFETY_CHK_DATA_INTEGRITY \
185 ((uint32_t) CSL_DSS_VID_SAFETY_ATTRIBUTES_CAPTUREMODE_VAL_DATACHECK)
196 #define CSL_DSS_SAFETY_CHK_FRAME_SKIP_NO \
197 ((uint32_t) CSL_DSS_VID_SAFETY_ATTRIBUTES_FRAMESKIP_VAL_DISABLE)
199 #define CSL_DSS_SAFETY_CHK_FRAME_SKIP_EVEN \
200 ((uint32_t) CSL_DSS_VID_SAFETY_ATTRIBUTES_FRAMESKIP_VAL_EVEN)
202 #define CSL_DSS_SAFETY_CHK_FRAME_SKIP_ODD \
203 ((uint32_t) CSL_DSS_VID_SAFETY_ATTRIBUTES_FRAMESKIP_VAL_ODD)
207 #define CSL_DSS_NUM_LUT_ENTRIES ((uint32_t) 256U)
210 #define CSL_DSS_MODULE_INVALID ((uint32_t) 0xFFU)
362 if(
NULL != safetyCfg)
Configuration for doing safety checks.
Definition: csl_dssTop.h:260
int32_t postOffset1
Definition: csl_dssTop.h:248
uint32_t startY
Definition: fvid2_dataTypes.h:1392
int32_t c02
Definition: csl_dssTop.h:228
int32_t c11
Definition: csl_dssTop.h:232
static void CSL_dssSafetyChkCfgInit(CSL_DssSafetyChkCfg *safetyCfg)
CSL_DssSafetyChkCfg structure init function.
Definition: csl_dssTop.h:359
int32_t preOffset3
Definition: csl_dssTop.h:246
uint32_t safetyChkEnable
Definition: csl_dssTop.h:261
int32_t preOffset2
Definition: csl_dssTop.h:244
int32_t c21
Definition: csl_dssTop.h:238
int32_t postOffset2
Definition: csl_dssTop.h:250
int32_t preOffset1
Definition: csl_dssTop.h:242
uint32_t startX
Definition: fvid2_dataTypes.h:1390
Structure containing coefficients for Color Space Conversion.
Definition: csl_dssTop.h:220
uint32_t seedSelectEnable
Definition: csl_dssTop.h:268
#define NULL
Define NULL if not defined.
Definition: csl_types.h:100
Structure containing size configuration.
Definition: fvid2_dataTypes.h:1401
uint32_t frameSkip
Definition: csl_dssTop.h:276
Structure containing position configuration - used in VCOMP and CIG.
Definition: fvid2_dataTypes.h:1389
int32_t c22
Definition: csl_dssTop.h:240
uint32_t thresholdValue
Definition: csl_dssTop.h:272
int32_t c10
Definition: csl_dssTop.h:230
static void CSL_dssCscCoeffInit(CSL_DssCscCoeff *cscCoeff)
CSL_DssCscCoeff structure init function.
Definition: csl_dssTop.h:335
uint32_t cscRange
Definition: csl_dssTop.h:221
UInt32 width
Definition: fvid2_dataTypes.h:1402
UInt32 height
Definition: fvid2_dataTypes.h:1404
Fvid2_PosConfig regionPos
Definition: csl_dssTop.h:279
int32_t c00
Definition: csl_dssTop.h:224
int32_t postOffset3
Definition: csl_dssTop.h:252
#define CSL_DSS_SAFETY_CHK_FRAME_SKIP_NO
No frames are skipped.
Definition: csl_dssTop.h:196
int32_t c01
Definition: csl_dssTop.h:226
#define CSL_DSS_CSC_RANGE_LIMITED
Limited range selected.
Definition: csl_dssTop.h:166
uint32_t safetyChkMode
Definition: csl_dssTop.h:265
#define CSL_DSS_SAFETY_CHK_FRAME_FREEZE_DETECT
Frame freeze detect enabled.
Definition: csl_dssTop.h:181
int32_t c20
Definition: csl_dssTop.h:236
Fvid2_SizeConfig regionSize
Definition: csl_dssTop.h:290
#define FALSE
Definition: csl_types.h:62
int32_t c12
Definition: csl_dssTop.h:234