TIFS Safety Checkers library APIs are integrated into the safety application to verify the firewall configuration and validate the FWL configuration against golden reference.
Features Supported
The module supports below API's for the application
- API to request TIFS to open firewall.
- API to generate Golden Reference using the list of firewall registers specified.
- API compares the Golden Reference with runtime firewall register values and return success or failure.
- API to request TIFS to close firewall.
SysConfig Features
Features NOT Supported
Important Usage Guidelines
Steps to update board configuration for TIFS Safety Checkers:
- Add below lines to the file " ${mcu_plus_sdk}/source/drivers/sciclient/sciclient_default_boardcfg/{board}/sciclient_defaultBoardcfg_security.c"
.sa2ul_auth_cfg = {
.subhdr = {
.size = 0,
},
.auth_resource_owner = 0,
.enable_saul_psil_global_config_writes = 0x5A,
.safety_host_present = 0x5A,
},
- Note
- host_id = 0x1E for mcu-r5f
- Use the following commands to build the Boardcfg changes For GP and HS-FS
cd ${mcu_plus_sdk}/tools/sysfw/boardcfg/
make SOC={board}
cd ${mcu_plus_sdk}
make scrub SOC={board}
make all SOC={board}
For HS-SE cd ${mcu_plus_sdk}/tools/sysfw/boardcfg/
make SOC={board} DEVICE_TYPE=HS
cd ${mcu_plus_sdk}
make scrub SOC={board} DEVICE_TYPE=HS
make all SOC={board} DEVICE_TYPE=HS
Example Usage
The following shows an example of TIFS Safety Checkers API usage
Include the below file to access the APIs
#include "../../src/safety_checkers_tifs.h"
Request the TIFS to open firewall
Uses the pointer to firewall configuration pFwlConfig as input and updates pFwlConfig with the register dump of the firewall registers specified.
Verify and save firewall configuration as Golden Reference
Compare the golden reference with runtime firewall register values and return success or failure.
while (i > 0)
{
if (status == SAFETY_CHECKERS_REG_DATA_MISMATCH)
{
SAFETY_CHECKERS_log("\n Firewall register mismatch with Golden Reference !!\r\n");
}
SafetyCheckersApp_softwareDelay();
i--;
}
if (status == SAFETY_CHECKERS_SOK)
{
SAFETY_CHECKERS_log("\n No firewall register mismatch with Golden Reference \r\n");
}
Request the TIFS to close firewall
API
API for TIFS Safety Checkers