AM62Px MCU+ SDK  12.00.00
SDL DCC Example

Introduction

This example demonstrates how to configure the DCC and use it to monitor clocks in the two supported modes (continuous and single-shot modes). It also demonstrates how to receive errors generated by DCC in the MCU and Main domain.

This example displays:

* Initializing the ESM to detect the DCC error event(s)
* Registration of application callback for notification of ESM error events for the MCU ESM instance
* Configuration of one MCU DCC instance to monitor a single clock in continuous mode
* Forcing of an error to create a DCC error event

The following methods can be used as a trigger for the DCC error event:

* Change ratio criterion for stable clocks
* Use Sciclient API to change clock dividers (with ratio criterion stable) to speed up clock
* Use Sciclient API to change clock dividers (with ratio criterion stable) to slow down clock
* Turn off power for the monitored input clock

Use Cases

Use Case Reference Clock Description
UC-1 HFOSC0 Configuration of MCU DCC instance in continuous mode and error event is forced
UC-2 HFOSC0 Configuration of MCU DCC instance in single-shot mode and completion with no errors
UC-3 HFOSC0 Configuration of MCU DCC instance in continuous mode and completion with no errors
UC-4 RC OSC Configuration of MCU DCC instance in single-shot mode and completion with no errors
UC-5 RC OSC Configuration of DCC instance in continuous mode and error event is forced
UC-6 RC OSC Configuration of DCC instance in continuous mode and error event is forced
UC-7 HFOSC0 Configuration of DCC instance in continuous mode and error event is forced
UC-8 RC OSC Configuration of DCC instance in continuous mode and completion with no errors
UC-9 HFOSC0 Configuration of DCC instance in single-shot mode and completion with no errors
UC-10 FICLK Configuration of DCC instance in single-shot mode and completion with no errors

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62px-sk
Example folder examples/sdl/dcc/dcc_app/

Steps to Run the Example

See Also

DCC

Sample Output

Shown below is a sample output when the application is run,

DCC Example Test Application
DCC_Test_init: Init WKUP ESM complete
USECASE: 0
Source clock: HFOSC0
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt
SDL DCC EXAMPLE TEST: Indicating clock drift/change
UC-0 Completed Successfully
USECASE: 1
Source clock: HFOSC0
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt
SDL DCC EXAMPLE TEST: No Clock Drift was observed
UC-1 Completed Successfully
USECASE: 2
Source clock: HFOSC0
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time
UC-2 Completed Successfully
USECASE: 3
Source clock: RC OSC
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt
SDL DCC EXAMPLE TEST: No Clock Drift was observed
UC-3 Completed Successfully
USECASE: 4
Source clock: RC OSC
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt
SDL DCC EXAMPLE TEST: Indicating clock drift/change
UC-4 Completed Successfully
USECASE: 5
Source clock: RC OSC
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt
SDL DCC EXAMPLE TEST: Indicating clock drift/change
UC-5 Completed Successfully
USECASE: 6
Source clock: RC OSC
Test clock: SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt
SDL DCC EXAMPLE TEST: Indicating clock drift/change
UC-6 Completed Successfully
USECASE: 7
Source clock: HFOSC0
Test clock: MAIN_SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and waiting for Error interrupt
SDL DCC EXAMPLE TEST: DCC Generated Error interrupt
SDL DCC EXAMPLE TEST: Indicating clock drift/change
UC-7 Completed Successfully
USECASE: 8
Source clock: RC OSC
Test clock: MAIN_SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: Enabling DCC and running for some time
UC-8 Completed Successfully
USECASE: 9
Source clock: HFOSC0
Test clock: FICLK
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt
SDL DCC EXAMPLE TEST: No Clock Drift was observed
UC-9 Completed Successfully
USECASE: 10
Source clock: FICLK
Test clock: MAIN_SYSCLK0
SDL DCC EXAMPLE TEST: Seed values calculation done.
SDL DCC EXAMPLE TEST: DCC Generated completion interrupt
SDL DCC EXAMPLE TEST: No Clock Drift was observed
UC-10 Completed Successfully
All tests have passed.