AM62Px MCU+ SDK  12.00.00
TIFS SAFETY CHECKERS APP

Introduction

TIFS Safety Checkers (TIFS-SC) library APIs can be used to get the firewall configuration and validate the same against the golden reference. The TIFS-SC has two stages, namely generation of firewall config and validation of firewall config. The SafetyCheckersApp_tifs demonstrates the usage of TIFS-SC library APIs.

To generate the firewall config, the user needs to first update the BoardCfg with the necessary values so that the TIFS will open the firewalls for the Safety host. The steps to do so are captured in the 'Important Usage Guidelines' section.

Once the BoardCfg is updated and the binaries are built, the Safety application needs to call 'tifsReqFwlOpen' to request TIFS to open the firewall register space. The application then sends a list of firewall ids that are to be monitored in the Safety Loop.

The complete list of permitted firewalls for a supported SOC can be found in 'tifs_checkers_fwl_config.h' present in the corresponding 'soc' folder of the TIFS-SC example. The user can modify the list based on which firewall ids need to be monitored. The safety checker iterates over the number of regions 'numRegions' specified in the tifs_checkers_fwl_config to generate the corresponding firewall config for a given firewall.

This list is used as input to 'SafetyCheckers_tifsGetFwlCfg' API along with it's size to generate the static firewall configuration. The Safety application then validates the generated firewall configuration and saves it as a Golden Reference in non-volatile memory. This completes stage 1.

The user should implement firewall based protection for golden reference and also create a checksum for the golden reference to ensure validity of the golden reference data.

The tifs_checkers_fwl_config.h can be regenerated using the Python script found under 'safety_checkers/utils/tifs_checkers_create_fwl_config.py'. The script uses a CSL file as input and generates the complete list of permitted firewalls for a given SoC.

In the validate phase, the Safety application provides the Golden Reference to the safety checker using the 'SafetyCheckers_tifsVerifyFwlCfg' API. The checker then the validates runtime firewall registers against the Golden Reference at defined intervals in a Safety Loop. The API return status indicates if there was a mismatch with the Golden Reference for any of the firewall ids. Finally the application must call 'tifsReqFwlClose' to request TIFS to close the firewall register space.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62px-sk
Example folder source/safety_checkers/examples/

Steps to Run the Example

See Also

TIFS_SAFETY_CHECKERS

Sample Output

Shown below is a sample output when the application is run,

Firewall open successful
Get firewall configuration successful
No firewall register mismatch with Golden Reference
Firewall close successful