AM62Px MCU+ SDK  12.00.00
PMIC Q&A watchdog interrupt example

Introduction

The example demonstrates the PMIC watchdog in Q&A mode which will generate a interrupt when the core fails to send the answers to the watchdog. The application configures the GPIO pins and the watchdog in the PMIC to send and receive the Q&A signals and the GPIO pin in the board to receive the interrupt from the PMIC upon failure. It services the watchdog for few iterations and stops sending the answers. Then, the core will wait to receive the PMIC interrupt. If the interrupt occurs, the test passes else fails.

Note
This example won't work in the debug mode as the user must not service the watchdog while in debug mode. Flash the application to get the expected result.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62px-sk
Example folder examples/drivers/pmic/pmic_qa_watchdog_interrupt

Steps

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • As it is a watchdog example, it cannot be loaded through CCS as it may fail in debug mode. It should be flashed and booted through SBL to get the expected results.
  • Refer Flash a Hello World example for flashing the application.

See Also

PMIC

Sample Output

Shown below is a sample output when the application is run,

Starting Q&A watchdog interrupt example !!
Configure PMIC GPIO pins for Q&A watchdog based on communication mode... DONE
Configure GPIO pin in the board to receive PMIC interrupt... DONE
Configure PMIC watchdog in Q&A mode... DONE
Started watchdog sequence... Sending answers to the watchdog...
Stopped sending watchdog answers... Waiting for the PMIC interrupt...
Received GPIO interrupt for PMIC watchdog error !!
PMIC Q&A watchdog interrupt mode test... DONE
All tests have passed!!