AM62Px MCU+ SDK  12.00.00
Hello World Project

Introduction

This example just does driver and board initialization and prints the string, Hello World! on UART console.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
mcu-r5fss0-0 freertos
wkup-r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am62px-sk
Example folder examples/empty/

Steps to Run the Example

Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

Sample Output

Shown below is a sample output when the application is run,

Hello World!