AM62Px MCU+ SDK  12.00.00
Empty Project

Introduction

This is an empty project provided for all cores present in the device. User can use this project to start their application by adding more SysConfig modules.

This application does driver and board init and just prints the pass string on the console. In case of the main core, the print is redirected to the UART console. For all other cores, CCS prints are used.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
mcu-r5fss0-0 freertos
wkup-r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am62px-sk
Example folder examples/empty/

Steps to Run the Example

Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

Sample Output

Shown below is a sample output when the application is run,

All tests have passed!!