AM62Px MCU+ SDK  12.00.00
Reset Isolation - MCU Domain

Introduction

The example demonstrates the MCU reset isolation in the use case when the MCU domain is running a safety application.

The example can be run in OSPI boot mode. On running the application the MCU R5 and logs a heartbeat message to theMCU UART.

On pressing the SOC Warm reset button (SW6), the MCU R5 which is reset isolated will keep on running, and the Main domain will undergo a warm reset. On reset the SBL would not reload the MCU R5 core again.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62px-sk
Example folder examples/drivers/safety/reset_isolation

Steps

Sample Output

Shown below is a sample output when the application is run,

################################ MCU R5 Log #######################################
I am running (MCU) !!:- 0
I am running (MCU) !!:- 1
I am running (MCU) !!:- 2
I am running (MCU) !!:- 3
I am running (MCU) !!:- 4
I am running (MCU) !!:- 5
Resetting Main domain !!
I am running (MCU) !!:- 6
I am running (MCU) !!:- 7
I am running (MCU) !!:- 8
I am running (MCU) !!:- 9
All tests have passed!!