AM62Px MCU+ SDK  12.00.00
I2C Temperature Read

Introduction

This example demonstrates probing of sensor via I2C and read data from it. The application reads data from the temperature sensor in the EVM. Application reads 20 samples from the sensor and exits.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
wkup-r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am62px-sk
Example folder examples/drivers/i2c/i2c_led_blink

Steps to Run the Example

Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Temperature sensor found at device address 0x48
[I2C] Sample 0: 39.000000 (celcius)
[I2C] Sample 1: 39.000000 (celcius)
[I2C] Sample 2: 39.000000 (celcius)
[I2C] Sample 3: 39.000000 (celcius)
[I2C] Sample 4: 39.000000 (celcius)
[I2C] Sample 5: 39.000000 (celcius)
[I2C] Sample 6: 39.000000 (celcius)
[I2C] Sample 7: 39.000000 (celcius)
[I2C] Sample 8: 39.000000 (celcius)
[I2C] Sample 9: 39.000000 (celcius)
[I2C] Sample 10: 39.000000 (celcius)
[I2C] Sample 11: 39.000000 (celcius)
[I2C] Sample 12: 39.000000 (celcius)
[I2C] Sample 13: 39.000000 (celcius)
[I2C] Sample 14: 39.000000 (celcius)
[I2C] Sample 15: 39.000000 (celcius)
[I2C] Sample 16: 39.000000 (celcius)
[I2C] Sample 17: 39.000000 (celcius)
[I2C] Sample 18: 39.000000 (celcius)
[I2C] Sample 19: 39.000000 (celcius)
All tests have passed!!