AM62Px MCU+ SDK  12.00.00
DSS Display Test

Introduction

This example tests the complete video pipeline configuration of DSS and displays it on a video port. DSS includes two video pipelines:

  • Video pipeline (VID)
  • Video lite pipeline (VIDL1)

The example allocates frame buffers and prepares test pattern for frame buffers for both pipelines in DDR. The example configures both the pipelines VID and VIDL for different attributes like input frame format, scaling, global alpha, and more. The mentioned VID and VIDL configurations are done as part of DSS driver sysconfig options shown below.

The example generates test pattern for both pipelines based on the frame format selected. The supported frame formats are RGB 16-bit, RGB 32-bit, RGB 64-bit, RGB 24-bit and YUV formats.

The example configures Zorder for overlay manager where VID and VIDL pipelines have Zorder 1 and 2 respectively. The Zorder can be changed using sysconfig option. The example configures scaling by default for VID pipeline. The VIDL pipeline does not support scaling for input frames.

The example configures DPI Panel for Video Port 2. It sets the video timing parameters for DPI output interface. The example also adds a Panel driver that configures a Sii9022a bridge driver for DPI to HDMI output on board.

The example integrates bootloading funtionality with SBL on OSPI bootmedia. It also integrates Device manager functionality. The SBL stage 2 thread boots all the cores along with HLOS like Linux. Refer SBL Booting Linux From OSPI for boot flow sequence.

Supported Combinations

Parameter Value
CPU + OS wkup-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62px-sk
Example folder examples/drivers/dss/dss_display_test

Steps to Run the Example

  • This example integrates SBL on OSPI bootmedia which needs to be flashed on the EVM flash, along with sample application images for MCU R5 CPUs, HSM M4F and Linux Appimage.
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg Linux echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • Update the wkup-r5 image in the flash config with dss_display_test image.
      # 2nd stage bootloader with DM is flashed at 0x80000 or to whatever offset your bootloader is configured for
      --file=../../examples/drivers/dss/dss_display_test/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/dss_display_test.release.appimage.hs_fs --operation=flash --flash-offset=0x80000
    
  • To flash to the EVM, refer to Flash a Hello World example . Only when giving the flash config file, point to the default_sbl_ospi_linux_hs_fs.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and Linux Appimage is already created, in Windows,
        cd C:/ti/mcu_plus_sdk/tools/boot
        python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • If Linux PC is used, assuming SDK is installed at ~/ti/mcu_plus_sdk
      cd ~/ti/mcu_plus_sdk
      python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
  • Switch to OSPI NOR BOOT MODE and power on the EVM.
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.

See Also

DSS

Sample Output

Sciserver Testapp Built On: Dec 7 2023 14:12:00
Sciserver Version: v2023.11.0.0REL.MCUSDK.MM.NN.PP.bb
RM_PM_HAL Version: vMM.NN.PP
Starting Sciserver..... PASSED
DispApp_init() - DONE !!!
DSS display application started...
Display create complete!!
Starting display ... !!!
Display in progress ... DO NOT HALT !!!
Underflow did not occur
Underflow did not occur
Sync Lost did not occur
Display delete complete!!
Number of frames = 300, elapsed msec = 5032, fps = 59.62
DispApp_deInit() - DONE !!!
DSS display test Passed!!

Display Output