AM62Px MCU+ SDK  12.00.00
BOOTLOADER

The Bootloader module provides APIs to write bootloader applications for various boot media like OSPI, UART, SOC memory etc.

Note
The bootloader driver is tested only in the context of a single thread and should be used only sequentially to boot cores to prevent potential errors and ensure stability. Also the current design of bootloader does not support parallel boot even when run in multiple threads.

Bootloader Migration Guidelines

While migrating to 11.00.00 MCU+ SDK, using the older example.syscfg file for bootloader examples with ospi dma enabled, can throw following error in gui, while running the command make syscfg-gui

Bootloader adds multiple udma instances

While using make command to build the example, it will throw following error

error: CONFIG_BOOTLOADER_FLASH_LINUX(/drivers/bootloader/bootloader) udmaDriver.$name: Duplicate name: 'CONFIG_UDMA0' also exists on instance(s) of UDMA
error: CONFIG_FLASH0(/board/flash/flash) serialFlashDriver.peripheralDriver.udmaDriver.$name: Duplicate name: 'CONFIG_UDMA0' also exists on instance(s) of UDMA
error: CONFIG_BOOTLOADER_FLASH_LINUX(/drivers/bootloader/bootloader) udmaBlkCopyChannel.$name: Duplicate name: 'CONFIG_UDMA_BLKCOPY_CH0' also exists on instance(s) of UDMA Block Copy Channel Configuration
error: CONFIG_FLASH0(/board/flash/flash) serialFlashDriver.peripheralDriver.udmaBlkCopyChannel.$name: Duplicate name: 'CONFIG_UDMA_BLKCOPY_CH0' also exists on instance(s) of UDMA Block Copy Channel Configuration
error: CONFIG_BOOTLOADER_FLASH_LINUX(/drivers/bootloader/bootloader) udmaDriver.instance: Same instance cannot be selected
error: CONFIG_FLASH0(/board/flash/flash) serialFlashDriver.peripheralDriver.udmaDriver.instance: Same instance cannot be selected

To fix this, update the example.syscfg, for every instance of bootloader define udma driver and udma block copy channel, refer the below lines to update example.syscfg

const udma = scripting.addModule("/drivers/udma/udma", {}, false);
const udma1 = udma.addInstance({}, false);
udma1.$name = "CONFIG_UDMA0";
flash1.serialFlashDriver.peripheralDriver.udmaDriver = udma1;
bootloader1.udmaDriver = udma1;
bootloader2.udmaDriver = udma1;
bootloader3.udmaDriver = udma1;
const udma_blkcopy_channel = scripting.addModule("/drivers/udma/udma_blkcopy_channel", {}, false);
const udma_blkcopy_channel1 = udma_blkcopy_channel.addInstance({}, false);
udma_blkcopy_channel1.$name = "CONFIG_UDMA_BLKCOPY_CH0";
flash1.serialFlashDriver.peripheralDriver.udmaBlkCopyChannel = udma_blkcopy_channel1;
bootloader1.udmaBlkCopyChannel = udma_blkcopy_channel1;
bootloader2.udmaBlkCopyChannel = udma_blkcopy_channel1;
bootloader3.udmaBlkCopyChannel = udma_blkcopy_channel1;

Migration Guide 11.02 to 12.00

Note
This section highlights linker changes from SDK 11.02 to 12.00.

<tt>gAtcmBaseAddr</tt> symbol required in SBL linker.cmd

  • SBL startup code (entered via -e_vectors_sbl) now references gAtcmBaseAddr to configure the ATCM base address at boot time.
  • Custom SBL linker.cmd files that specify -e_vectors_sbl as the entry point must define this symbol, or the linker will report an undefined symbol error.

Old linker.cmd:

--heap_size=0x8000
-e_vectors_sbl

New linker.cmd:

--heap_size=0x2000
/* ATCM base address - required when using -e_vectors_sbl entry point */
gAtcmBaseAddr = 0x78000000;
-e_vectors_sbl
Note
If ATCM is also needed for SBL heap and interrupt stacks, add the ATCM region to MEMORY and relocate .sysmem and stack sections to ATCM. An MPU entry for ATCM is needed to be added to example.syscfg as well if so used.
MEMORY
{
ATCM (RWIX) : ORIGIN = 0x78000000 LENGTH = 0x8000
HSM_RAM (RWIX) : ORIGIN = 0x43C00000 LENGTH = 0x3E000
}
SECTIONS
{
.sysmem: {} palign(8) > ATCM
GROUP {
.irqstack: {. = . + __IRQ_STACK_SIZE;} align(8)
.fiqstack: {. = . + __FIQ_STACK_SIZE;} align(8)
} > ATCM
GROUP {
.svcstack: {. = . + __SVC_STACK_SIZE;} align(8)
.abortstack: {. = . + __ABORT_STACK_SIZE;} align(8)
} > ATCM
}
const mpu_armv7_ATCM = mpu_armv7.addInstance();
mpu_armv7_ATCM.$name = "ATCM_SOC";
mpu_armv7_ATCM.baseAddr = 0x78000000;
mpu_armv7_ATCM.size = 15;

Features Supported

  • OSPI Boot
  • MEM Boot (Boot media is SOC memory)
  • API to parse multicore appimage
  • Separate APIs to boot self and non-self cores

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • Bootloader instance name
  • Boot Media to be used
  • Boot Image offset

R5 Dual Core Support

RBL boots the R5 in eFUSE default, which is split mode. SBL (Secondary Boot Loader) follows the same and keeps the R5s in split mode. As of now the lock step configuration of dual R5 is not supported from bootloader.

Example Usage

Include the below file to access the APIs

#include <stdio.h>

Instance Open Example

gBootloaderHandle = Bootloader_open(0, NULL);
DebugP_assert(gBootloaderHandle != NULL);

Booting Cores Example

status = Bootloader_parseMultiCoreAppImage(gBootloaderHandle, &gBootImageInfo);
if(SystemP_SUCCESS == status && gBootloaderHandle != NULL)
{
{
gBootImageInfo.cpuInfo[CSL_CORE_ID_M4FSS0_0].clkHz = Bootloader_socCpuGetClkDefault(CSL_CORE_ID_M4FSS0_0);
status = Bootloader_bootCpu(gBootloaderHandle, &gBootImageInfo.cpuInfo[CSL_CORE_ID_M4FSS0_0]);
}
{
gBootImageInfo.cpuInfo[CSL_CORE_ID_M4FSS0_0].clkHz = Bootloader_socCpuGetClkDefault(CSL_CORE_ID_R5FSS1_0);
status = Bootloader_bootCpu(gBootloaderHandle, &gBootImageInfo.cpuInfo[CSL_CORE_ID_R5FSS1_0]);
}
{
gBootImageInfo.cpuInfo[CSL_CORE_ID_R5FSS1_1].clkHz = Bootloader_socCpuGetClkDefault(CSL_CORE_ID_R5FSS1_1);
status = Bootloader_bootCpu(gBootloaderHandle, &gBootImageInfo.cpuInfo[CSL_CORE_ID_R5FSS1_1]);
}
{
gBootImageInfo.cpuInfo[CSL_CORE_ID_R5FSS0_0].clkHz = Bootloader_socCpuGetClkDefault(CSL_CORE_ID_R5FSS0_0);
gBootImageInfo.cpuInfo[CSL_CORE_ID_R5FSS0_1].clkHz = Bootloader_socCpuGetClkDefault(CSL_CORE_ID_R5FSS0_1);
/* Reset self cluster, both Core0 and Core 1. Init RAMs and run the app */
status = Bootloader_bootSelfCpu(gBootloaderHandle, &gBootImageInfo);
}
}

Instance Close Example

Bootloader_close(gBootloaderHandle);

API

APIs for BOOTLOADING CPUs

status
uint32_t status
Definition: tisci_lpm.h:1
Bootloader_bootSelfCpu
int32_t Bootloader_bootSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
NULL
#define NULL
Define NULL if not defined.
Definition: csl_types.h:100
Bootloader_parseMultiCoreAppImage
int32_t Bootloader_parseMultiCoreAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse Multicore Appimage.
Bootloader_close
void Bootloader_close(Bootloader_Handle handle)
Close bootloader driver.
Bootloader_bootCpu
int32_t Bootloader_bootCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to boot a non-self CPU.
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
Bootloader_socCpuGetClkDefault
uint32_t Bootloader_socCpuGetClkDefault(uint32_t cpuId)
Get the default clock of a particular CPU in the AM62x SOC.
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:183
bootloader.h
Bootloader_open
Bootloader_Handle Bootloader_open(uint32_t instanceNum, Bootloader_Params *openParams)
Open bootloader driver.