AM62Px MCU+ SDK  12.00.00
Understanding the bootflow and bootloaders

Introduction

Note
This scope of this document is to cover the bootflow of the secondary bootloader (SBL) available as part of the MCU+ SDK. SPL bootflow is covered as part of 'Boot Flow' section in PSDK Linux documentation.

Booting user defined applications on a SOC involves multiples steps as listed below,

  • Firstly, there are multiple steps involved to convert a user application, created using a compiler+linker toolchain, into a binary format that is suitable to be booted by the SOC
  • Next, we need to flash this binary to the EVM flash
  • Finally, when the SOC is powered on, the previously flashed binary is executed.
  • After powering on the EVM, the bootflow takes place mainly in two steps
    • ROM boot, in which the ROM bootloader boots a secondary bootloader or an SBL
    • SBL boot in which the secondary bootloader boots the application
  • Note, that a system application itself can consist of multiple CPU specific application binaries that all collaborate together to realize the overall system goal.

This section details these steps and gives an overview of the bootloaders to understand the process better.

Additional References

See also these additional pages for more details and examples about the boot flow,

Preparing the application for boot

Note
To see the exact sequence of steps in which applications and secondary bootloader (SBL) are converted from compiler generated .out files to boot images, see the makefile makefile_ccs_bootimage_gen that is included in every example and secondary bootloader (SBL) CCS project.
If you are using makefile based build, then see the file named makefile in the example folder.

Shown below are the different steps that are done to convert the compiler+linker generated application .out into a format suitable for flashing and booting

  • For each CPU, the compiler+linker toolchain is used to create the application .out "ELF" file which can be loaded and run via CCS
  • The below "post build" steps are then used to convert the application .out into a "flash" friendly format
    • For each CPU, out2rpc is used to convert the ELF .out to a binary file containing only the loadable sections. This is called a RPRC file.
    • multiCoreGen is then used to combine all the RPRC files per CPU into a single .appimage file which is a concatenation of the individual CPU specific RPRC files.
  • This .appimage is then flash to the EVM

Post build steps

Flashing the application for boot

  • Once the application image (.appimage) is created one needs to copy or flash these to a supported boot media so that the application can start executing once the SOC is powered ON
  • When flashing the application we also need to flash a bootloader or SBL image.
  • See Flashing Tools for detailed steps that are done to flash a user application

Booting the application

After a SBL and application image is flashed, shown below is the high level boot flow, after the SOC is powered on.

HIGH LEVEL BOOTFLOW

ROM Boot

  • As soon as the EVM is powered ON, the ROM bootloader or RBL starts running. The RBL is the primary bootloader.
  • Depending on which boot mode is selected on the EVM, the RBL will load the secondary bootloader or SBL from a boot media (OSPI flash, SD card or via UART).
  • ROM also loads TIFS binary to TIFS Cortex M4, board configuration data to the predefined locations.
  • Rest of the booting is done by the SBL.
  • The RBL expects the image it boots (SBL in our case) to always be signed. Refer Booting Tools for more information on signing scripts.

SBL Boot

  • The SBL is essentially an example application of the bootloader library.
  • We call it a secondary bootloader because it is booted by the RBL, which is the primary bootloader.
  • An SBL typically does a bunch of SOC specific initializations and proceeds to the application loading.
  • In case of AM62PX EVM, the SBL loads the DM Firmware to DM R5F.
  • In case of AM62PX EVM, the SBL stage 2 will boot the cores in following order, 1st HSM 2nd MCU and 3rd A53. This order is followed across all the bootloader examples.
  • To change the bootloader order for different use cases, follow the below steps
    • Step1 Open the Syscfg gui to configure the bootloader order. Refer Using SDK with SysConfig,to know how to use Syscfg gui.
    • Step2 Select the bootloader instance.
      Opening Bootloader Instance
    • Step3 Add bootloader instance for different cores, depending on the order in which the core has to be booted. The order in the below image is HSM MCU and Linux, the order in which the instance is displayed.
      Adding Bootloader Instance
  • Depending on the type of SBL loaded, SBL looks for the multicore appimage (refer Booting Tools for more on multicore appimage) of the application binary at a specified location in a boot media.
  • If the appimage is found, the multicore appimage is parsed into multiple RPRCs. These are optimized binaries which are then loaded into individual CPUs.
  • Each RPRC image will have information regarding the core on which it is to be loaded, entry points and multiple sections of that application binary
  • The SBL uses this information to initialize each core which has a valid RPRC. It then loads the RPRC according to the sections specified, sets the entry points and releases the core from reset. Now the core will start running

Secondary Bootloaders

Depending on the boot media from which we load the application binary, we have multiple SBLs like sbl_ospi,sbl_uart etc. A bare minimum SBL called the sbl_null is also included which aids the users to load their applications via CCS.

SBL NULL

  • The sbl_null is a secondary bootloader which doesn't load any application binary, but just does the SOC initialization and puts all the cores in WFI (Wait For Interrupt) mode.
  • This is referred to as the SOC initialization binary, refer Flash SOC Initialization Binary for more on this.

SBL UART

  • The sbl_uart is a secondary bootloader which receives the multicore appimage via UART, stores it in memory and then does the parsing, core initialization etc.
  • To boot an application using the sbl_uart, you can refer to UART Bootloader Python Script subsection. Detailed steps on the usage is mentioned in the same subsection.

SBL OSPI LINUX

  • The sbl_ospi_linux is a secondary bootloader which boots Linux on A53 core and RTOS/NORTOS application on R5, M4 cores.
  • To boot Linux and RTOS/NORTOS applications using sbl_ospi_linux, the Linux appimage (see Linux Appimage Generator Tool) and the RTOS/NORTOS application images needs to be flashed at a particular location in the OSPI NOR flash memory.
  • This location or offset is specified in the SysConfig of the sbl_ospi_linux application.
  • To flash an application (or any file in fact) to a location in the OSPI flash memory, follow the steps mentioned in Basic steps to flash files

SBL EMMC LINUX

  • The sbl_emmc_linux is a secondary bootloader which boots Linux on A53 core and RTOS/NORTOS application on R5, M4 cores from eMMC.
  • To boot Linux and RTOS/NORTOS applications using sbl_emmc_linux, the Linux appimage (see Linux Appimage Generator Tool) and the RTOS/NORTOS application images needs to be flashed at a particular location in the eMMC.
  • This location or offset is specified in the SysConfig of the sbl_emmc_linux application.
  • To flash an application (or any file in fact) to a location in the eMMC, follow the steps mentioned in Basic steps to flash files

Preparing the SBL for boot

The SBL is like any other application, created using the same compiler and linker toolchain. However the steps to convert the application .out into a bootable image are different for SBL as listed below

  • The SBL entry point needs to be different vs other applications. On AM62PX after power-ON ROM boots the SBL and sets the entry point of SBL to R5FSS0-0. This is done by specifying a different entry point -e_vectors_sbl in the linker command file for the SBL application.
  • Other special factors for SBL application are listed below
    • The linker command file for SBL has to place vectors at address 0x43C00000 and this is the entry point for the SBL.
    • Nothing should be placed in ATCM or BTCM
    • Only the region 0x43C00000 to 0x43C3C800 should be used by SBL code, data, stack etc
  • After building, the SBL application .out file is first converted to a binary format .bin using the GCC objcopy tool.
    • This copies the loadable sections from the .out into a binary image stripping all symbol and section information.
    • If there are two loadable sections in the image which are not contiguous then objcopy fills the gaps with 0xFF.
    • It is highly recommended to keep all loadable sections together within a SBL application.
  • This .bin file is then signed using the Signing Scripts to create the final .tiimage bootable image.
    • A default key is used for this.
    • This is a ROM bootloader requirement and is needed even on a non-secure device.
  • This .tiimage file can then be flashed or copied to a boot image using the Flashing Tools