SBL UART Linux
Introduction
This bootloader does SOC initializations and attempts to boot a multicore appimage received over UART via XMODEM. The image file is sent using a python script (See UART Bootloader Python Script). Once image is received, the SBL then parses it, splits it into RPRCs for each core applicable. Each core is then initialized, RPRC image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders
Note
This example is loaded with UART bootmode. A53 SPL loaded by this example will pick this up and boot up in UART bootmode. This can be changed by calling SOC_setDevStat() in main.c
Note
Once the A53 SPL begins execution in UART bootmode(C is printed), the U-Boot image can be sent over UART0(/dev/ttyUSBx for Linux and COMx for Windows). The U-boot image is located at tools/boot/linuxAppimageGen/board. Send the U-boot image using xmodem over UART0. If SD Card is present, U-boot will load the linux filesystem from SD Card.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup-r5fss0-0 nortos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/boot/sbl_uart_linux |
Refer Enabling DDR inline ECC enablig inline ECC
Steps to Run the Example
Build the example
Since this is a bootloader and is used as a SOC initialization binary, the example will be run every time you boot an application using this example. It is generally run from a boot media (OSPI Flash, SD Card or over UART) unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles).
Create Linux Appimage
Note
Change DEVICE_TYPE to HS in ${SDK_INSTALL_PATH}/devconfig/devconfig.mak and then generate Linux Appimage for HS-SE device.
Create a Linux Appimage containing the Linux binaries (ATF, OPTEE, A53 SPL)
This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen after setting the PSDK path in file
config.makRefer Linux Appimage Generator Tool for more details
Run the example
Note
For HS-SE device, use default_sbl_uart_hs.cfg as the cfg file.
Note
For HS-FS device, use default_sbl_uart_hs_fs.cfg as the cfg file.
Run the following command from the {MCU_PLUS_SDK_INSTALLATION_PATH}/tools/boot
For am62px-sk
python uart_bootloader.py -p /dev/ttyUSB0 --cfg=sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_uart_linux.cfg
Here /dev/ttyUSB0 can be changed to COM port like’COM4’ incase of Windows.
Note
The above config file will flash till u-boot. U-Boot can load kernel from any bootmedia, refer to Processor SDK Linux user guide for more details.
See Also
Device-Specific Overlay
For AM62A, AM62P, AM62X2-SK-LP, and AM62X-SK devices:
The overlay is applied to load the ATF at 0x80000000.
The overlay code is:
/dts-v1/; /plugin/; / { #address-cells = <0x02>; #size-cells = <0x02>; fragment@0 { #address-cells = <0x02>; #size-cells = <0x02>; ranges; target-path = "/reserved-memory/tfa09e780000"; __overlay { #address-cells = <0x02>; #size-cells = <0x02>; ranges; reg = <0x00 0x80000000 0x00 0x80000>; }; }; };
Sample Output
Since this SBL receives the appimage over UART using XMODEM protocol, it doesn’t print anything to the console so as not to corrupt the XMODEM transport.