PMIC trigger watchdog reset example
Introduction
The example demonstrates the PMIC watchdog in trigger mode which will generate a warm reset when the core fails to send the trigger to the watchdog. The application configures the GPIO pin and the watchdog in the PMIC to receive the trigger signal. It services the watchdog for few iterations and stops sending the trigger signal. Then, the core will wait for sometime based on the reset threshold value configured in the watchdog for the warm reset to occur. If the warm reset occurs, the test passes else fails.
Note
This example won’t work in the debug mode as the user must not service the watchdog while in debug mode. Flash the application to get the expected result.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/pmic/pmic_trigger_watchdog_reset |
Steps
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
As it is a watchdog example, it cannot be loaded through CCS as it may fail in debug mode. It should be flashed and booted through SBL to get the expected results.
Refer Flash a Hello World example for flashing the application.
Or use default_pmic_trigger_watchdog_reset_hs_fs.cfg for HS-FS device, default_pmic_trigger_watchdog_reset_hs.cfg for HS-SE device.
Set bootmode to UART BOOT MODE and flash the binary using the following command from {SDK_INSTALLTION_PATH}/tools/boot
python uart_uniflash.py -p /dev/ttyUSB0 --cfg=../../examples/drivers/pmic/pmic_trigger_watchdog_reset/am62px-sk/default_pmic_trigger_watchdog_reset_hs_fs.cfg
Power OFF and change the boot mode to OSPI NOR BOOT MODE
Logs should appear at the MCU_UART0
See Also
Sample Output
Shown below is a sample output when the application is run,
Starting trigger watchdog reset example !!
Configure GPIO trigger watchdog pin in the PMIC... DONE
Configure PMIC watchdog in Trigger mode... DONE
Started watchdog sequence... Sending watchdog trigger signal to the PMIC...
Stopped sending watchdog trigger signal... Waiting for the warm reset to occur...
Warm reset has occurred due to watchdog failure!!
All tests have passed!!