PMIC trigger watchdog interrupt example

Introduction

The example demonstrates the PMIC watchdog in trigger mode which will generate a interrupt when the core fails to send the trigger to the watchdog. The application configures the GPIO pin and the watchdog in the PMIC to receive the trigger signal and the GPIO pin in the board to receive the interrupt from the PMIC upon failure. It services the watchdog for few iterations and stops sending the trigger signal. Then, the core will wait to receive the PMIC interrupt. If the interrupt occurs, the test passes else fails.

Note

This example won’t work in the debug mode as the user must not service the watchdog while in debug mode. Flash the application to get the expected result.

Supported Combinations

Parameter

Value

CPU + OS

mcu-r5fss0-0 freertos

Toolchain

ti-arm-clang

Board

am62px-sk

Example folder

examples/drivers/pmic/pmic_trigger_watchdog_interrupt

Steps

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

  • As it is a watchdog example, it cannot be loaded through CCS as it may fail in debug mode. It should be flashed and booted through SBL to get the expected results.

  • Refer Flash a Hello World example for flashing the application.

See Also

PMIC

Sample Output

Shown below is a sample output when the application is run,

Starting trigger watchdog interrupt example !!
Configure GPIO trigger watchdog pin in the PMIC... DONE
Configure GPIO pin in the board to receive PMIC interrupt... DONE
Configure PMIC watchdog in Trigger mode... DONE
Started watchdog sequence... Sending watchdog trigger signal to the PMIC...
Stopped sending watchdog trigger signal... Waiting for the PMIC interrupt...
Received GPIO interrupt for PMIC watchdog error !!
PMIC trigger watchdog interrupt mode test... DONE
All tests have passed!!