MCSPI Performance 8 Bit
Introduction
This Master application demonstrates the data transfer in master mode with performance measurment.
McSPI is configured in Tx Only mode with FIFO enabled for Tx.
Word Length tested is 8 bits.
SPI CLK Frequency used is 12 MHZ.
Number of Words is 5.
Data is transmitted on D0 pin.
Data transmission is in polled mode.
To modify the example to use main domain SPI, refer Accessing main and wakeup domain peripherals from MCU domain
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
mcu-r5fss0-0 freertos |
CPU + OS |
mcu-r5fss0-0 nortos |
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Boards |
am62px-sk |
Example folder |
examples/drivers/mcspi/mcspi_performance_8bit |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
Refer Flash a Hello World example for flashing the application.
See Also
Sample Output
Shown below is a sample output when the application is run,
[MCSPI] Performance Example Started...
----------------------------------------------------------
McSPI Clock 50000000 Hz
----------------------------------------------------------
Data Width Data Length Transfer Time (micro sec)
8 5 2.40
----------------------------------------------------------
All tests have passed!!