ECAP APWM mode

Introduction

This example uses the ECAP in APWM mode to generate a PWM signal.

The example does the below

  • Configures ECAP in APWM mode and configures values in period and compare registers

  • Waits for the specified time using the ECAP ISR.

External Connections

AM62PX-SK

  • The signal can be probed on Pin 7 (C25/GPIO1_30) of the User Expansion Connector (J4) on the base board.

Supported Combinations

Parameter

Value

CPU + OS

mcu-r5fss0-0 freertos

Toolchain

ti-arm-clang

Boards

am62px-sk

Example folder

examples/drivers/ecap/ecap_apwm_mode/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).

  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

  • Establish connections as mentioned in External Connections section

See Also

ECAP

Sample Output

Shown below is a sample output when the application is run,

ECAP APWM Mode Test Started ...
ECAP APWM Test Passed!!
All tests have passed!!