DSS Display Share
Introduction
Display subsystem supports sharing of display between multiple hosts as it provides separate register space (common* region) for each host to programming display controller and also an unique interrupt line for each host. HLOS like Linux owns one or more of the video planes with video port (along with corresponding overlay manager) associated with these planes being owned and controlled by a remote core.
This example shares the DSS with high level OS like linux. The example uses one DSS pipeline (VIDL) and keeps the other pipeline for HLOS (VID).
The example uses DSS0 instance with VIDL pipeline, OVR1 overlay and VP1 videoport. The overlay manager is configured with Zorder 1 for VID pipeline and Zorder 2 for VIDL pipeline. The example acts as master for controlling DSS and expects linux to use VID pipeline. The VID and VIDL pipeline are overlayed together as per mentioned zorder above.
The Display sharing feature can be enabled by using below shown sysconfig option.
DSS Display Share Configuration
The example integrates early splash of image along with SBL on OSPI bootmedia, Device Manager and Interprocessor communication functionality. The bootloader IPC and Display run on separate tasks. The Display task displays a splash image with alpha blending and finally switches to display sharing task, where it ping pongs tell tale frames. The SBL stage 2 thread boots all the cores along with HLOS like Linux. Refer SBL Booting Linux From OSPI for boot flow sequence.
The example configures OLDI LVDS panel for Video Port 1. Please refer SK-LCD1 for panel details. The Video port timinng parameters are configured with respect to SK-LCD1. Timing parameters can be configured using sysconfig option.
The example implements a firewall function to configure firewall for DSS register regions used by the driver to ensure display-sharing functionality. This provides access for read, write, cache, and debug DSS register regions for the core running the DSS driver in RTOS context and provides only read access to the application core running HLOS like Linux. The example also configures a firewall for frame buffer memory region used in RTOS context for display sharing. This provides read, write, cache, and debug access to the DSS peripheral and core running the DSS driver in the RTOS context. This blocks access from all other entities in SoC from accessing the frame buffer memory region.
Note
To support display sharing on Linux, there exists a device tree overlay which should be applied to kernel device tree to enable DSS sharing on Linux. The overlays are k3-am62p5-sk-microtips-mf101hie-panel.dtbo and k3-am62p5-sk-dss-shared-mode.dtbo. Use tisdk-display-cluster-image-am62pxx-evm.wic.xz image to flash linux root file system. This default wic image launches Cluster demo as shown in display output below. Please refer Processor SDK Linux documentation for more details.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup-r5fss0-0 freertos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/drivers/dss/dss_display_share |
Steps to Run the Example
This example integrates SBL on OSPI bootmedia which needs to be flashed on the EVM flash, along with sample application images for MCU R5 CPUs, HSM M4F and Linux Appimage.
For HS-FS device, use default_sbl_ospi_linux_hs_fs_splash_screen.cfg as the cfg file.
There is a default flash config file as shown below which flashes this SBL and the display share application
${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_ospi_linux_hs_fs_splash_screen.cfgTo flash to the EVM, refer to Flash a Hello World example . Only when giving the flash config file, point to the
default_sbl_ospi_linux_hs_fs_splash_screen.cfgshown above.Example, assuming SDK is installed at
C:/ti/mcu_plus_sdkand this example and IPC application is built using makefiles, and Linux Appimage is already created, in Windows,cd C:/ti/mcu_plus_sdk/tools/boot python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_ospi_linux_hs_fs_splash_screen.cfgIf Linux PC is used, assuming SDK is installed at
~/ti/mcu_plus_sdkcd ~/ti/mcu_plus_sdk python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/{{ VAR_BOARD_NAME_LOWER }}/default_sbl_ospi_linux_hs_fs_splash_screen.cfgSwitch to OSPI NOR BOOT MODE and power on the EVM.
Attention
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
See Also
Sample Output
Sciserver Testapp Built On: Dec 7 2023 14:12:00
Sciserver Version: v2023.11.0.0REL.MCUSDK.MM.NN.PP.bb
RM_PM_HAL Version: vMM.NN.PP
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.MM.NN.PP.bb (Dec 7 2023 14:12:16):
DispApp_init() - DONE !!!
DSS display share application started...
Display create complete!!
Starting display ... !!!
Display in progress ... DO NOT HALT !!!
DSS display share Passed!!
Number of elapsed frames = 300, elapsed msec = 4999, fps = 60.01
[IPC RPMSG ECHO] Message exchange started with RTOS cores !!!
[IPC RPMSG ECHO] Remote Core waiting for messages at end point 13 ... !!!
[IPC RPMSG ECHO] Remote Core waiting for messages at end point 14 ... !!!
Number of elapsed frames = 300, elapsed msec = 5010, fps = 59.88
[IPC RPMSG ECHO] All echoed messages received by main core from 1 remote cores !!!
[IPC RPMSG ECHO] Messages sent to each core = 100000
[IPC RPMSG ECHO] Number of remote cores = 1
[IPC RPMSG ECHO] Total execution time = 3591085 usecs
[IPC RPMSG ECHO] One way message latency = 17955 nsec
Number of elapsed frames = 300, elapsed msec = 5011, fps = 59.87
Number of elapsed frames = 300, elapsed msec = 5011, fps = 59.87
Display Output
Display Output