SOC | Supported CPUs | EVM | Host PC |
---|---|---|---|
AM62P | MCU R5F, WKUP R5F | SK-AM62P-LP EVM (referred to as am62px-sk in code) | Windows 10 64b or Ubuntu 22.04 64b |
Feature | Module |
---|---|
Updated the EMMC tuning for robustness | EMMC |
Tools/Components | Supported CPUs | Version |
---|---|---|
Code Composer Studio | MCU-R5F, WKUP-R5F | 12.7.0 |
SysConfig | MCU-R5F, WKUP-R5F | 1.20.0, build 3587 |
TI ARM CLANG | MCU-R5F, WKUP-R5F | 3.2.2.LTS |
GCC AARCH64 | A53 | 9.2-2019.12 |
FreeRTOS Kernel | MCU-R5F, WKUP-R5F | 10.6.1 |
TIFS | NA | 09.02.08 |
OS | Supported CPUs | SysConfig Support |
---|---|---|
FreeRTOS Kernel | MCU-R5F, WKUP-R5F | NA |
FreeRTOS POSIX | MCU-R5F | NA |
No RTOS | MCU-R5F, WKUP-R5F | NA |
Module | Supported CPUs | SysConfig Support | OS support |
---|---|---|---|
Address Translate | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
Cache | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
Clock | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
CycleCounter | MCU-R5F, WKUP-R5F | NA | FreeRTOS, NORTOS |
Debug | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
Heap | MCU-R5F, WKUP-R5F | NA | FreeRTOS, NORTOS |
Hwi | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
MPU | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
Semaphore | MCU-R5F, WKUP-R5F | NA | FreeRTOS, NORTOS |
Task | MCU-R5F, WKUP-R5F | NA | FreeRTOS |
Timer | MCU-R5F, WKUP-R5F | Yes | FreeRTOS, NORTOS |
SBL Mode | Supported CPUs | SysConfig Support | PHY Support | DMA Support | OS support |
---|---|---|---|---|---|
OSPI NOR | WKUP-R5F | Yes | Yes | Yes | NORTOS |
EMMC | WKUP-R5F | Yes | NA | NA | NORTOS |
UART | WKUP-R5F | Yes | NA | No | NORTOS |
SDL Module | Supported CPUs | SysConfig Support |
---|---|---|
MCRC | MCU-R5F | No |
ESM | MCU-R5F | No |
VTM | MCU-R5F | No |
DCC | MCU-R5F | No |
ECC | MCU-R5F | No |
RTI | MCU-R5F | No |
POK | MCU-R5F | No |
STOG | MCU-R5F | No |
MTOG | MCU-R5F | No |
POK | MCU-R5F | No |
PBIST | MCU-R5F | No |
LBIST | MCU-R5F | No |
ROM_CHECKSUM | MCU-R5F | No |
Peripheral | Domain | Supported CPUs | SysConfig Support |
---|---|---|---|
DDR | Main | WKUP-R5F | Yes |
ECAP | Main | MCU-R5F | Yes |
EPWM | Main | MCU-R5F, WKUP-R5F | Yes |
DSS | Main | WKUP-R5F | Yes |
GPIO | MCU | MCU-R5F, WKUP-R5F | Yes |
Main | MCU-R5F, WKUP-R5F | Yes | |
I2C | Main | MCU-R5F, WKUP-R5F | Yes |
MCU | MCU-R5F, WKUP-R5F | Yes | |
Wakeup | MCU-R5F, WKUP-R5F | Yes | |
IPC | Main | MCU-R5F, WKUP-R5F | Yes |
MCAN | MCU | MCU-R5F | Yes |
MCASP | Main | WKUP-R5F | Yes |
MCSPI | Main | MCU-R5F, WKUP-R5F | Yes |
MCU | MCU-R5F, WKUP-R5F | Yes | |
Pinmux | Main | MCU-R5F, WKUP-R5F | Yes |
MCU | MCU-R5F, WKUP-R5F | Yes | |
Wakeup | MCU-R5F, WKUP-R5F | Yes | |
SOC | NA | MCU-R5F, WKUP-R5F | Yes |
SCIClient | NA | MCU-R5F, WKUP-R5F | Yes |
UART | Main | MCU-R5F, WKUP-R5F | Yes |
MCU | MCU-R5F, WKUP-R5F | Yes | |
Wakeup | WKUP-R5F | Yes |
ID | Head Line | Module | Applicable Releases |
---|---|---|---|
SITSW-4243 | Enabling DM firmware log causing the DM to go to abort | DM | 09.02.00 onwards |
SITSW-4337 | Bootloader_socInitR5FAtcmBtcm function uses global ATCM address resulting in CBASS error | SBL | 08.04.00 onwards |
SITSW-4345 | A53 core freq is limited to 1250MHz in bootloader | SBL | 08.04.00 onwards |
SITSW-4499 | TISCI_MSG_KEY_WRITER message is not part of secure context in SCI client | DM | 09.02.00 onwards |
SYSFW-6831 | DM self_reset operation stuck in abort_self_reset sometimes | DM | 08.04.00 onwards |
SYSFW-7183 | Warm reset after system LPM entry/exit results in u-boot/DM hang | DM | 09.02.00 onwards |
SYSFW-7251 | Enabling DM UART traces in boardcfg causes abort in DeepSleep resume path | DM | 09.02.00 onwards |
SYSFW-7315 | Extra bypass step in boot time pll init routine | DM | 09.02.00 onwards |
SYSFW-7327 | DM self reset goes to abort with logs enabled in SBL flow | DM | 09.02.00 onwards |
SYSFW-7370 | pm init functions are missing proper return values | DM | 09.02.00 onwards |
SYSFW-7375 | Firewall Exception during devices_init function in DM | DM | 09.02.00 onwards |
ID | Head Line | Module | Reported in release | Workaround |
---|---|---|---|---|
MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 07.03.00 | Use bash for windows as part of git for windows or don't use -j option |
SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 08.06.00 | None. |
S.No | Head Line | Module |
---|---|---|
1 | The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK | NA |
2 | LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. | Bootloader |