Feature | Module |
OSPI NOR tuning algorithm is updated for robustness | OSPI |
DDR inline ECC support added | DDR |
APIs to measure DDR usage is added | DDR |
UDMA Examples are added for MCU R5F | UDMA |
Dhryston benchmark examples added for MCU R5F | Examples |
Memcpy benchmark examples added for MCU R5F and DM R5F | Examples |
Security examples: Firewall exception handling, Configure/Read firewalls | Examples |
TIFS, RM and PM safety checker library and examples are added | Safety Checker |
ECAP and EPWM support is added for MCU-R5F | ECAP, EPWM |
MCU reset isolation support is added | Safety |
MCU only LPM support added | IPC |
LBIST and PBIST of MCU R5F is done on SBL before booting MCU R5F | SBL |
PLL Configuration sequence updated to latest recommendation | DM |
HSM infrastructure updates | TIFS |
ID | Head Line | Module | Applicable Releases |
SITSW-2776 | OSPI is broken on SBL Falcon mode | OSPI | 09.01.00 onwards |
SITSW-3100 | MCASP Driver Stop, then MCASP Start does not work | MCASP | 09.01.00 onwards |
SITSW-3353 | UART traces from TIFS M4 are not available | UART | 09.01.00 onwards |
SITSW-3443 | Sysconfig error in MMCSD module on setting Card Type to NO_DEVICE | MMCSD | 09.01.00 onwards |
SITSW-3448 | Issue in the clean target of Linux Appimage makefile on windows | Build | 09.01.00 onwards |
SITSW-3489 | HSM & Linux Appimage build fails with gmake from CCS in Windows | Build | 09.01.00 onwards |
SITSW-3600 | FwdStatus is set as SCISERVER_FORWARD_MSG for secure messages from DM R5 core | DM | 09.01.00 onwards |
SITSW-3606 | OSPI Phase Delay Value is wrong | OSPI | 09.01.00 onwards |
SITSW-3610 | clock mux changes are lost after deepsleep entry/exit | DM | 09.01.00 onwards |
SITSW-3612 | EMMC boot is failing after warm reset | EMMC | 09.01.00 onwards |
SITSW-3645 | Default DMA configs are using invalid ring ranges | UDMA | 09.01.00 onwards |
SITSW-3678 | Failure in importing any example in CCS from AM62P MCU+ SDK | Build | 09.01.00 onwards |
SITSW-3795 | Early splash screen not coming under 200 ms with fast boot | DSS | 09.01.00 onwards |
SITSW-3823 | EMMC CSL header has issue withrespect to STRBSEL | EMMC | 09.01.00 onwards |
SITSW-3845 | Errata i2310 causes erroneous set of UART timeout interrupt | UART | 09.02.00 onwards |
SITSW-3901 | fwl isolation example configures ownership for background region instead of foreground region | Security Examples | 09.01.00 onwards |
SITSW-3902 | Bootloader DMA has redundent cache management policies | SBL | 09.01.00 onwards |
SITSW-3950 | DDR: sdram index field is not cleared before writing | DDR | 09.01.00 onwards |
SITSW-3965 | DDR DFI timeout interrupts are happening in idle state | DDR | 09.01.00 onwards |
SITSW-4234 | SBL Uart Linux does not acknowledge 'end of file' message | SBL | 09.00.00 onwards |
PROC_SDL-7045 | ESM example is failing. | SDL | 09.02.00 onwards |
PROC_SDL-7267 | SDL_POK_Inst and SDL_PRG_Inst macros defined twice in POK driver | SDL | 09.02.00 onwards |
PROC_SDL-7128 | Remove ESM Error Pin Counter Value Register from static register read API | SDL | 09.02.00 onwards |
SYSFW-6763 | TISCI_MSG_SET_DEVICE_RESETS message returns success for invalid device reset range | DM | 08.03.00 onwards |
SYSFW-7056 | Implement New PLL sequence Proposed by HW team | DM | 08.03.00 onwards |
SYSFW-6941 | TISCI_MSG_SYS_RESET fails for negative testcase | DM | 08.03.00 onwards |
SYSFW-6892 | TISCI Clock api returns success for invalid Clock ID | DM | 08.03.00 onwards |
SYSFW-5266 | LPM: USB must not remove reset isolation until LPSC has been reenabled | DM | 08.03.00 onwards |
SYSFW-6805 | TISCI_MSG_QUERY_FW_CAPS is giving NACK when send over secure queue | TIFS | 09.00.00 onwards |
SYSFW-6879 | clock_stop API in baremetal disables all configurable interrupts | TIFS | 09.01.00 onwards |
ID | Head Line | Module | Reported in release | Workaround |
MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 09.01.0 | Use bash for windows as part of git for windows or don't use -j option |
SITSW-2269 | DeepSleep Low power mode (LPM) is not supported if the DM R5 is used for a general purpose application. | DM | 09.01.00 | None. |
PROC_SDL-6326 | Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F | LBIST | 09.02.00 | None |
PROC_SDL-7044 | ECC is not supported for some instances. These are SDL_DSS_DSI0_K3_DSS_DSI_DSI_TOP_ECC_AGGR_SYS SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR | SDL | 09.01.00 | None. Support will be added in future release. |
SYSFW-5992 | Unable to set exact pixel clock for OLDI LCD display / HDMI Pixel clock | DM | 08.05.00 | Avoid gving range for SET_CLOCK, use exact values for min, max and target |
SYSFW-6369 | DM unable to enter deep sleep mode when booting in SBL flow | DM | 08.03.00 | None. |
SYSFW-6432 | Set device API doesn't return Error when PD is in transition state | DM | 08.03.00 | None. |
SYSFW-7183 | Warm reset after system LPM entry/exit results in u-boot/DM hang | DM | 09.02.00 | None. |
SYSFW-6426 | Ownership of a firewall region can be transferred to an invalid host | TIFS | 08.03.00 | None. |