AM62Px MCU+ SDK  09.02.00
Flash a Hello World example

Attention
Flashing a application will overwrite the SOC init application that was flashed earlier. So if you want to load and run from CCS again, you will need to do the SOC init steps again. See SOC Initialization for more details.
As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
Note
See also Flashing Tools for more details on the flashing tools.

Introduction

In this step we will flash the application that we have build and run using CCS to the EVM flash. We can then boot this application without being connected to CCS via JTAG.

Getting ready to flash the application

  • A quick recap of steps done so far that are needed for the flashing to work
    • Make sure the UART port used for terminal is identified as mentioned in Setup UART Terminal
    • Make sure python3 is installed as mentioned in Python3
    • Make sure you have the EVM power cable and UART cable connected as shown in Cable Connections
  • Build the hello world application as mentioned in Build a Hello World example
  • As part of the build process in the final step a file with extension .appimage.hs_fs is generated. This is the file we need to flash.
    • When building with makefiles and single-core projects, this file can be found here (shown for hello world example),
      • For MCU R5F
         ${SDK_INSTALL_PATH}/examples/hello_world/am62px-sk/mcu-r5fss0-0_freertos/ti-arm-clang/hello_world.release.appimage.hs_fs
        
      • For DM R5F (WKUP R5F)
         ${SDK_INSTALL_PATH}/examples/hello_world/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/hello_world.release.appimage.hs_fs
        
    • When building with CCS projects, this file can be found here (shown for hello world example),
      • For MCU R5F
         ${CCS_WORKSPACE_PATH}/hello_world_am62px-sk_mcu-r5fss0-0_freertos_ti-arm-clang/Release/hello_world_am62px-sk_mcu-r5fss0-0_freertos_ti-arm-clang.appimage.hs_fs
        
      • For DM R5F (WKUP R5F)
        ${CCS_WORKSPACE_PATH}/hello_world_am62px-sk_r5fss0-0_freertos_ti-arm-clang/Release/hello_world_am62px-sk_wkup-r5fss0-0_freertos_ti-arm-clang.appimage.hs_fs
        
    • NOTE: The folder name and file name in path can have "release", "Release" or "debug", "Debug" based on the profile that the application is built with.
  • Next, we need to list the files to flash in a flash configuration file. A default configuration file can be found at below path. You can edit this file directly or take a copy and edit this file.
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
    Note
    For HS-FS device, use default_sbl_ospi_linux_hs_fs.cfg as the cfg file.
  • Edit below line in the config file to point to your application .appimage file. Give the absolute path to the .appimage file or path relative to ${SDK_INSTALL_PATH}/tools/boot. Make sure to use forward slash / in the filename path.
    • For MCU R5F
      --file=../../examples/drivers/ipc/ipc_rpmsg_echo_linux/am62px-sk/mcu-r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage.hs_fs --operation=flash --flash-offset=0x800000
      
    • For DM R5F
      --file=../../examples/drivers/ipc/ipc_rpmsg_echo_linux/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage.hs_fs --operation=flash --flash-offset=0xC0000
      
  • This file will additionally also list the flashing application that is run on the EVM and a OSPI flash bootloader that also needs to be flashed. You can keep this unchanged if you have not modified these applications.
  • Save and close the config file.

Building Linux app image and HSM app image

The linux and HSM app images are to be generated to flash along with your application for MCU R5.

LinuxAppImage

  • Ensure the AM62P Processor SDK Linux path is correct in the ${SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen/board/{board_name}/config.mak file.
  • Go to ${SDK_INSTALL_PATH}/tools/boot/linuxAppimageGen on terminal
  • Run the following command to build the linux app image.
    • For SK-AM62P-LP
      make BOARD=am62px-sk all

HSMAppImage

  • Go to ${SDK_INSTALL_PATH}/tools/boot/HSMAppimageGen on terminal
  • Run the following command to build the HSM app image.
    • For SK-AM62P-LP
      make BOARD=am62px-sk all

Flashing the application

  • Build all the binaries
    • For Linux
      make DEVICE=am62px -sj
    • For Windows
      gmake DEVICE=am62px -sj
  • POWER-OFF the EVM
  • Set boot mode to UART BOOTMODE as shown in below image

UART BOOT MODE
  • POWER-ON the EVM
  • You should see character "C" getting printed on the UART terminal every 2-3 seconds as shown below

UART output in UART BOOT MODE
  • Close the UART terminal as shown below. This is important, else the UART script in next step wont be able to connect to the UART port.

Close UART terminal
Note
For HS-FS device, use default_sbl_ospi_linux_hs_fs.cfg as the cfg file.
  • Open a command prompt and run the below command to flash the SOC initialization binary to the EVM.
      cd ${SDK_INSTALL_PATH}/tools/boot
      python uart_uniflash.py -p COM13 --cfg=sbl_prebuilt/am62px-sk/default_sbl_ospi_linux_hs_fs.cfg
    
    • Here COM13 is the port name of the identified UART port in Windows.
    • On Linux,
      • The name for UART port is typically something like /dev/ttyUSB0
      • On some Linux systems, one needs to use python3 to invoke python3.x, just python command may invoke python 2.x which will not work with the flashing script.
  • When the flashing is in progress you will see something like below

Flash in progress
  • After all the flashing is done, you will see something like below
      Parsing config file ...
      Parsing config file ... SUCCESS. Found 9 command(s) !!!
    
      Executing command 1 of 9 ...
      Found flash writer ... sending sbl_prebuilt/am62px-sk/sbl_uart_uniflash_stage1.release.hs_fs.tiimage
      Sent flashwriter sbl_prebuilt/am62px-sk/sbl_uart_uniflash_stage1.release.hs_fs.tiimage of size 286255 bytes in 28.78s.
    
      Executing command 2 of 9 ...
      Command arguments : --file=../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62px-sk/wkup-r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage.hs_fs --operation=flash --flash-offset=0x0
      Sent ../../examples/drivers/boot/sbl_uart_uniflash_multistage/sbl_uart_uniflash_stage2/am62px-sk/wkup-r5fss0-0_nortos/ti-arm-clang/sbl_uart_uniflash_stage2.release.appimage.hs_fs of size 123939 bytes in 15.21s.
      [STATUS] SUCCESS !!!
    
      Executing command 3 of 9 ...
      Command arguments : --operation=flash-phy-tuning-data
      Sent flash phy tuning data in 3.87s.
      [STATUS] SUCCESS !!!
    
      Executing command 4 of 9 ...
      Command arguments : --file=sbl_prebuilt/am62px-sk/sbl_ospi_linux_stage1.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
      Sent sbl_prebuilt/am62px-sk/sbl_ospi_linux_stage1.release.hs_fs.tiimage of size 325935 bytes in 33.63s.
      [STATUS] SUCCESS !!!
    
      Executing command 5 of 9 ...
      Command arguments : --file=../../examples/drivers/ipc/ipc_rpmsg_echo_linux/am62px-sk/wkup-r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage.hs_fs --operation=flash --flash-offset=0x80000
      Sent ../../examples/drivers/boot/sbl_ospi_linux_multistage/sbl_ospi_linux_stage2/am62px-sk/wkup-r5fss0-0_nortos/ti-arm-clang/sbl_ospi_linux_stage2.release.appimage.hs_fs of size 139483 bytes in 16.13s.
      [STATUS] SUCCESS !!!
    
      Executing command 6 of 9 ...
      Command arguments : --file=../../examples/drivers/ipc/ipc_rpmsg_echo_linux/am62px-sk/mcu-r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage.hs_fs --operation=flash --flash-offset=0x800000
      Sent ../../examples/drivers/ipc/ipc_rpmsg_echo_linux/am62px-sk/mcu-r5fss0-0_freertos/ti-arm-clang/ipc_rpmsg_echo_linux.release.appimage.hs_fs of size 52687 bytes in 7.97s.
      [STATUS] SUCCESS !!!
    
      Executing command 7 of 9 ...
      Command arguments : --file=../../tools/boot/HSMAppimageGen/board/am62px-sk/hsm.appimage.hs_fs --operation=flash --flash-offset=0x240000
      Sent ../../tools/boot/HSMAppimageGen/board/am62px-sk/hsm.appimage.hs_fs of size 9646 bytes in 3.94s.
      [STATUS] SUCCESS !!!
    
      Executing command 8 of 9 ...
      Command arguments : --file=../../tools/boot/linuxAppimageGen/board/am62px-sk/linux.appimage.hs_fs --operation=flash --flash-offset=0x1200000
      Sent ../../tools/boot/linuxAppimageGen/board/am62px-sk/linux.appimage.hs_fs of size 733151 bytes in 71.71s.
      [STATUS] SUCCESS !!!
    
      Executing command 9 of 9 ...
      Command arguments : linuxAppimageGen/board/am62px-sk/u-boot.img --operation=flash --flash-offset=0x280000
      Sent linuxAppimageGen/board/am62px-sk/u-boot.img of size 1160651 bytes in 121.0s.
      [STATUS] SUCCESS !!!
    
    
      All commands from config file are executed !!!
    
  • If flashing has failed, see Flash tool error messages and solutions, and resolve the errors.
  • If flashing is successful, do the next steps ...

Running the flashed application

  • POWER-OFF the EVM
  • Switch the EVM boot mode to OSPI mode as shown below,

OSPI BOOT MODE
  • Re-connect the UART terminal in CCS window as shown in Setup UART Terminal
  • POWER-ON the EVM
  • You should see the application output in MCU UART terminal as below
      Hello World!
    
  • You should see the application output in WKUP UART terminal as below
      Sciserver Testapp Built On: Feb 21 2023 17:57:59
      Sciserver Version: v2023.01.0.0REL.MCUSDK.08.06.00.16+
      RM_PM_HAL Version: REL.MCUSDK.08.06.00.16
      Starting Sciserver..... PASSED
      GTC freq: 200000000
      Hello World!
    
  • You should see the following SBL output on the main UART terminal as below.
      SYSFW Version 9.0.5--v09.00.05 (Kool Koala)
      SYSFW revision 0x9
      DMSC ABI revision 3.1
    
      [BOOTLOADER_PROFILE] Boot Media       : FLASH
      [BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
      [BOOTLOADER_PROFILE] Boot Image Size  : 184 KB
      [BOOTLOADER_PROFILE] Cores present    :
      wkup-r5f0-0
      [BOOTLOADER PROFILE] System_init                      :      39175us
      [BOOTLOADER PROFILE] Drivers_open                     :        191us
      [BOOTLOADER PROFILE] Board_driversOpen                :         87us
      [BOOTLOADER PROFILE] Sciclient Get Version            :       9893us
      [BOOTLOADER PROFILE] App_loadImages                   :       4541us
      [BOOTLOADER PROFILE] App_loadSelfcoreImage            :       9288us
      [BOOTLOADER_PROFILE] SBL Total Time Taken             :      70975us
    
      Image loading done, switching to application ...
      Starting MCU-r5f and 2nd stage bootloader
    
      SYSFW Version 9.0.5--v09.00.05 (Kool Koala)
      SYSFW revision 0x9
      DMSC ABI revision 3.1
    
      [BOOTLOADER_PROFILE] Boot Media       : FLASH
      [BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
      [BOOTLOADER_PROFILE] Boot Image Size  : 1001 KB
      [BOOTLOADER_PROFILE] Cores present    :
      mcu-r5f0-0
      hsm-m4f0-0
      wkup-r5f0-0
      a530-0
      [BOOTLOADER PROFILE] System_init                      :       1801us
      [BOOTLOADER PROFILE] Drivers_open                     :        224us
      [BOOTLOADER PROFILE] Board_driversOpen                :         86us
      [BOOTLOADER PROFILE] Sciclient Get Version            :       9910us
      [BOOTLOADER PROFILE] App_loadImages                   :       2289us
      [BOOTLOADER PROFILE] App_loadSelfcoreImage            :       9051us
      [BOOTLOADER PROFILE] App_loadLinuxImages              :      40933us
      [BOOTLOADER PROFILE] App_loadDSPImages                :       9623us
      [BOOTLOADER_PROFILE] SBL Total Time Taken             :      73921us
    
      Image loading done, switching to application ...
      Starting linux and RTOS/Baremetal applications
    
  • Congratulations now the EVM is flashed with your application and you don't need CCS anymore to run the application.